P9222-R enables manufacturers to complement their earbuds, hearing aids and other small, battery-powered devices with wireless charging cases

2019年10月2日

SAN JOSE, Calif., October 2, 2019 – Integrated Device Technology, Inc. (IDT), a wholly owned subsidiary of Renesas Electronics Corporation (TSE: 6723), today announced the availability of its new P9222-R wireless power receiver, the industry’s smallest and optimized for wireless charging cases used to charge earbuds, hearing aids and other small, battery-powered consumer devices. Unlike other available solutions, the P9222-R is cost-optimized, highly efficient, feature rich and proven in high-volume applications with major consumer electronics manufacturers.

The P9222-R receiver is ideal for wireless charging cases of up to 5W thanks to its combination of ultra-compact size (just 2.28 mm × 3.38 mm) and extremely low power consumption (less than 50mW). The new receiver is also supported by an EVK reference design with a small 30 × 30 mm coil.

“Our new P9222-R wireless power receiver enables manufacturers to get to market faster with wireless charging cases for earbuds, hearing aids and other small, battery-powered consumer devices thanks to its combination of programmability, small size and low power consumption,” said Chris Stephens, vice president and general manager of IDT’s Wireless Power division. “With the P9222-R Rx, manufacturers can simultaneously meet their key goals of maximizing battery life while decreasing the overall size of their devices.”

A unique feature of the P9222-R is ping detection, which prevents overheating by reducing power consumption at the end of the battery’s charging cycle. Complementing this, the P9222-R is optimized for efficient light load operation to further minimize temperature rise. The new Rx also features an extremely low under-voltage lockout (UVLO) threshold, which enables fast charging over an extended area even when a wireless power transmitter’s digital ping strength is weak – providing consumers with a better user experience.

The extremely flexible and customizable P9222-R helps accelerate time-to-market and reduces time spent in Qi certification. The key to this flexibility is the P9222-R’s integrated 32-bit ARM Cortex-M0 processor, which offers a high level of programmability and design parameters that can be easily configured through the I2C interface or an external EEPROM.

The P9222-R wireless power receiver is available today. Visit idt.com/P9222-R for more information and to request samples.

IDT is the global leader in wireless power solutions for both the Power Receivers (PRx) used in smartphones and other applications, as well as the Power Transmitters (PTx) used in charging pads and automotive in-car applications. Visit idt.com/wirelesspower to learn more about IDT’s wireless power solutions.

About IDT

Integrated Device Technology, Inc., a wholly owned subsidiary of Renesas Electronics Corporation (TSE: 6723), develops system-level solutions that optimize its customers’ applications. IDT’s market-leading products in RF, high performance timing, memory interface, real-time interconnect, optical interconnect, wireless power and smart sensors are among the company’s broad array of complete mixed-signal solutions for the communications, computing, consumer, automotive and industrial segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. Additional information about IDT can be found at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

© 2019, Integrated Device Technology, Inc. IDT  and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc., and its worldwide subsidiaries. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

この記事をシェアする