Build Differentiated HMI Solutions On Top of the Renesas RZ/A MPU Hardware Platform with Express Logic ThreadX® RTOS and Middleware

2014年4月2日

EE LIVE, SAN JOSE, Calif., April 1, 2014 — Renesas Electronics America, a leading supplier of advanced semiconductor solutions, and Express Logic, Inc., the worldwide leader in royalty-free real-time operating systems (RTOSs), announce the new RZ Express program—an optimized package of high-performance microprocessors (MPUs), easy-to-use RTOS, and comprehensive middleware solutions ideal for high-resolution displays used in the design of human-machine interface (HMI) applications.

The RZ Express program offers embedded designers developing a commercial application with any Renesas RZ/A1 high-performance MPU the chance to obtain a valuable single-product license for Express Logic’s ThreadX® RTOS. This includes any Express Logic middleware components required to complete the application—NetX™, USBX™, FileX®, and GUIX™. Additionally, free software support and maintenance is provided for 90 days.* The RZ Express program brings together a powerful hardware platform and a leading commercial RTOS to help reduce design and execution risk by providing a proven path to high- performance user interfaces.

“Using the Express Logic RTOS and middleware, including GUIX, helps designers quickly and effectively build differentiated HMI solutions on top of the Renesas RZ/A1 hardware platform,” said Ritesh Tyagi, vice president of marketing for Renesas Electronics America. “The RZ/A1 MPUs have been optimized for HMI applications and, when used with GUIX and the Express Logic middleware, provide an optimal solution for high-resolution displays.”

Renesas RZ/A series of MPUs combine a high-performance ARM® Cortex-A9 processor with up to an industry-leading 10MB of on-chip RAM to support faster device control, digital audio and video-signal processing, and much more. The large on-chip RAM removes the need for external SDRAM, enabling low-power, cost-effective embedded display applications at up to WXGA resolution. The RZ/A MPUs can also drive two displays and execute code in-place from cost-effective QSPI flash memory.

“Today’s end user expects to manage an embedded device through an intuitive human-machine interface,” noted William E. Lamie, president of Express Logic. “RZ Express provides engineers with the fully-integrated tools they need to design a system that is responsive, powerful, and graphically pleasing all within a minimal footprint. What’s more, RZ Express provides this robust software support free, saving development teams thousands of dollars otherwise needed for such high-quality software.”

RTOS/Middleware

Express Logic’s ThreadX RTOS is deployed in over two billion electronic products, most of which are powered by ARM-based processors. ThreadX and Express Logic’s related middleware provide priority-based, pre-emptive, real-time scheduling, messaging, IPv4/IPv6 networking, USB Host/Device, and GUI software support for these systems. The Express Logic products strongly complement the Renesas RZ/A MPU.

The RZ Express promotion is valid only in the Americas (North America, South America and Central America). Qualified customers* can request a single-product license by registering their project with Renesas. For more information, or to apply for the program, visit http://am.renesas.com/RZExpress.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

For more information, follow Renesas Electronics America at@RenesasAmerica on Twitter and http://www.facebook.com/RenesasAmerica.

About Express Logic

Headquartered in San Diego, CA, Express Logic offers the most advanced run-time solutions for deeply embedded applications, including the popular ThreadX® RTOS, the high-performance NetX™ TCP/IP stack, the FileX® embedded FAT-compatible file system, the USBX™ Host/Device USB protocol stack, and the GUIX™ graphical user interface development toolkit. Most products from Express Logic include full source code and all have no run-time royalties.

For more information about Express Logic solutions, please visit the Web site at www.expresslogic.com, call 1-858-613-6640, or e-mail inquiries to [email protected].

Remarks
All other product and service names that appear in this newsflash are trademarks or registered trademarks of their respective owners.

*Terms and conditions apply. See http://am.renesas.com/RZExpress/Terms_and_Conditions for more details and RZ Express program qualification criteria.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする