2011年2月9日

TOKYO, Japan, February 9, 2011 — Renesas Mobile Corporation, an innovative supplier of advanced cellular semiconductor solutions and platforms, today announces an end-to-end Long Term Evolution (LTE) demonstration using 1800 Megahertz (MHz) spectrum together with Nokia Siemens Networks at Mobile World Congress 2011 from February 14-17, 2011.

The demonstration features commercial base station equipment from Nokia Siemens Networks and Renesas Mobile's test platform using a highly integrated LTE triple-mode modem. The companies' collaboration on LTE at 1800MHz (LTE1800) fully conforms to 3GPP (Third Generation Partnership Project) radio performance requirements, and illustrates that LTE1800 will soon be made commercially available.

Much of the initial focus in LTE development has been in the use of newly allocated frequency bands and has overlooked the importance of reusing existing spectrum. The 1800MHz band, which is widely used today for GSM, is becoming a key band for LTE deployments. It is particularly well suited to be used for high capacity and high throughput broadband wireless networks, as many operators have significant bandwidth on the band, allowing 20MHz configurations.

Renesas Mobile and Nokia Siemens Networks have been amongst the first to prove the technical feasibility of LTE technology at 1800MHz in an end-to-end configuration covering network and user equipment.

“The LTE 1800MHz frequency band combines good coverage with large bandwidth”, said Thorsten Robrecht, head of Network Systems product management, Nokia Siemens Networks. “It will be extremely important for LTE adoption especially in countries where additional spectrum for LTE will not be available. We are now demonstrating LTE1800 with Renesas Mobile to show what a cost-effective route to commercial LTE it is. This continues our close co-operation to ensure a smooth market introduction.”

“A deep, long-term relationship with leading infrastructure vendors such as Nokia Siemens Networks is very important to ensure that our roadmaps and technology deployment plans are aligned”, said Heikki Tenhunen, Senior Vice President, Renesas Mobile Corporation. “We have been working closely with Nokia Siemens Networks for many years to bring technology including LTE1800 to market that benefits consumers and operators.”

About Renesas Mobile Corporation

Renesas Mobile Corporation (RMC) is a wholly owned subsidiary of Renesas Electronics Corporation (TSE: 6723) and offers advanced and innovative products and services for mobile phones, car infotainment solutions, consumer electronics and industrial applications. Renesas Mobile's mission is to develop, productize and deliver communications centric semiconductor chipsets and complete hardware and software platforms built on these chipsets to meet the needs of our customers in these markets. Renesas Mobile provides complete cellular chipset platform solutions including powerful applications processors, leadership and industry reference cellular modems, highly integrated radio frequency devices and intelligent power management solutions. Renesas Mobile offers our customer complete system and software expertise to develop flagship devices more rapidly.

(Remarks)
Names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする