Renesas RZ/G2M Awarded Arm SystemReady IR 1.1 Certification

Renesas RZ/G2M Awarded Arm SystemReady IR 1.1 Certification

The Renesas RZ/G2M platform is the first RZ/MPU platform to be officially certified by Arm as compliant with SystemReady IR 1.1, a set of interoperability specifications targeting edge and IoT devices.

Single MCU Solution for Safety-Related Applications Using TrustZone Blog

Single MCU Solution for Safety-Related Applications Using TrustZone

Learn how RA 32-bit MCUs enable implementing a Class C application on a single microcontroller.

Power Up Your SPI Transfers

Power Up Your SPI Transfers

This blog looks at how we can automate a series of SPI transfers using the command sequencer implemented on many RA 32-bit MCU devices.

Solution for debugging and profiling multiple automotive devices

車載マルチデバイスのデバッグ/プロファイリングソリューション

協調動作が必要なマルチデバイス環境におけるソフトウェア開発の課題を解消するためのソリューションを紹介します。

Looking for a Reliable, Ready-to-Use Gigabit Industrial Ethernet Solution? Blog

Looking for a Reliable, Ready-to-Use Gigabit Industrial Ethernet Solution?

Gigabit speed and its associated frequencies require sophisticated schematics and PCB design. Renesas’ Gigabit Industrial Ethernet SoM solution contains all of the needed mission-critical components.

Reducing Noise Issues in Microcontroller Systems Blog

Reducing Noise Issues in Microcontroller Systems - Part 4

In this blog, we look at some of the features implemented on RA microcontrollers that can help create reliable applications in the face of noise.

Renesas AI Panel Recap: Semiconductor Industry Is Pulling AI Across a Diversity of End Uses and Applications

半導体産業が多様な用途と応用でAIをリードする

半導体を活用してAIが普及していく期待と、半導体業界の中で設計やテストにAIが活用されている現状と展望を、キーマンらがパネルディスカッションした内容を紹介します。

 Accelerate Your Automotive Innovations with the R-Car S4 SoC Low Cost Evaluation Board Starter Kit Blog

Accelerate Your Automotive Innovations with the R-Car S4 SoC Low-Cost Evaluation Board Starter Kit

As the automotive industry is challenged to introduce software-defined vehicles (SDVs), it is crucial to have a low-cost and easy-to-use development environment for rapid software development.

Ethernet Evolution for Industrial Applications

産業用アプリケーションにおけるイーサネットの進化

産業用イーサネットは、インダストリー4.0の決定論とリアルタイム制御を可能にするさまざまなネットワーキング・プロトコルをサポートし、重要な役割を果たしています。

Giving Customers the Options to Make or Buy SoM and/or SBC to Accelerate Design Cycle

SOM/SBCの製造または購入という選択肢が、顧客の設計サイクルを加速させます

システムオンモジュール(SOM)やシングルボードコンピュータ(SBC)を使用する主な利点は、必要な知識やリソースを分割できることです。開発サイクルの加速に役立つ、すぐに使えるSOMとSBCの利点を詳しく掘り下げてみていきます。