SmartBond™ DA14695 Bluetooth Low Energy 5.2 Development Kit Pro
The DA14695 Development Kit Pro is ideal for software developers who want total control over their software development and want to keep an eye on the power consumption...
The Renesas SmartBond™ Flash Programmer tool lets the user program a flash device for the DA1453x, DA14585/586, and DA1469x SoCs (System on Chip).
This tool allows the user to:
The DA14695 Development Kit Pro is ideal for software developers who want total control over their software development and want to keep an eye on the power consumption...
This USB development kit gives users the flexibility to develop applications in a small and portable form factor. The USB board has an on-board debugger, which in...
The DA14531 SmartBond TINY™ Development Kit Pro (DA14531-00FXDEVKT-P) is the most ideal way to quickly and easily get started developing applications and products using...
The DA14531 SmartBond TINY™ USB Development Kit gives you all the flexibility to develop applications in a small and portable form factor.
This kit offers a low-cost...
DA14592-016FDEVKT-P 低功耗蓝牙开发套件 Pro 包括主板、子板和电缆。 该套件专为软件应用开发和功耗测量而设计。
DA14592 是一款双核蓝牙 5.2 SoC,具有 256kB 嵌入式闪存,可在超低功耗水平下运行,提供世界一流的射频性能。 DA14592 采用 FCQFN 和 WLCSP 封装。