DA16200 Ultra-Low Power Wi-Fi Modules Development Kit
The DA16200 development kit is the most ideal way to quickly and easily get started developing applications and products using ultra-low power Wi-Fi.
If you are...
DA16200 片上系统 (SoC) 是全球首款为一直在线的 Wi-Fi 物联网设备提供一年以上电池续航时间的 Wi-Fi SoC。 DA16200 是一款低功耗 Wi-Fi 网络 SoC,即使是持续连接 Wi-Fi 网络的设备,其电池寿命也能大大延长。 大多数应用中可实现一年以上的电池寿命。 SoC 的续航时间业界领先,所以无需在输出功率或续航方面有所权衡。 该芯片还具有非常强大的物联网安全性,包括 WPA3 和 TLS,用于 Wi-Fi 和更高堆栈层的身份验证和加密。 DA16200 是完全卸载的器件,因此整个 Wi-Fi 和 TCP/IP 网络堆栈,甚至最终产品应用代码都可以在芯片上运行,无需外部 CPU 或 MCU。 另外,小型廉价 MCU 也可以发送 DA16200 命令,而 SoC 仍将执行完整的卸载网络堆栈功能。
DA16200模块 是 DA16200 超低功耗 Wi-Fi SoC 的完美补充。
无需在 Wi-Fi 端开发任何复杂软件,即可快速获取 DA16200/DA16600 系列先进的低功耗功能。 了解更多信息,请访问 DA16200 Wi-Fi AT 命令集 页面。
Software title
|
Software type
|
公司
|
---|---|---|
DA16200 Wi-Fi AT Command Set Simple and fast Wi-Fi implementation using a comprehensive suite of AT-Commands for the DA16200 Wi-Fi and DA16600 Wi-Fi/Bluetooth LE combo products.
|
IDE and Coding Tool | 瑞萨电子 |
1 item
|
The DA16200 development kit is the most ideal way to quickly and easily get started developing applications and products using ultra-low power Wi-Fi.
If you are...
使用 DA16200 低功耗 Wi-Fi 开发套件加速物联网开发。 基于 VirtualZero™ 的 DA16200 开发套件使开发物联网应用程序变得简单快捷。
如果您想要开发电池供电的物联网应用,DA16200 Wi-Fi 开发者套件能让您在几分钟内入门。 这款 Wi-Fi 开发套件非常完备,可让您全面了解和评估超低功耗...
LP WiFi Click is a compact add-on board that represents an ultra-low power Wi-Fi solution. This board features the DA16200, a fully integrated Wi-Fi module with...
SparkFun has teamed up with Arm and Renesas to provide you with this Qwiic WiFi Shield based around the DA16200 module. The DA16200 is a fully integrated Wi-Fi module...
The SparkFun MicroMod DA16200 Function Board adds a fully integrated Wi-Fi module with a 40MHz crystal oscillator, 32.768KHz RTC, Lumped RF filter, 4MB flash memory,...
The SparkFun DA16200 Thing Plus utilizes a highly integrated ultra-low power Wi-Fi system-on-chip (SoC) from Renesas that allows users to develop Wi-Fi and IoT...
The CK-RA6M5 cloud kit enables users to securely connect to the cloud and explore the features of the Cortex®-M33 based RA6M5 group of MCUs and cloud services. With...
The CK-RX65N cloud kit enables users to securely connect to the cloud and explore the features of the Renesas RXv2 core based RX65N MCU Group and cloud services.
With...
The US159-DA16600EVZ is a highly integrated ultra-low-power Wi-Fi + Bluetooth® Low Energy Combo Pmod module that provides a convenient way to add both low power Wi-Fi...
该电路板提供丰富的连接功能,包括移动屏幕的 Wi-Fi 镜像和蓝牙® 低功耗(LE)连接,以及仪表盘所需的低成本解决方案,如摄像头图像显示、指示灯和 TFT 亮度控制。
AS043-FGSLEAKPOC2Z 可燃气体泄漏检测仪是一个电池供电的独立系统,该系统使用低功耗 Wi-Fi 通信实现无线连接。 该解决方案使用 ZMOD4410 气体传感器检测可燃气体的泄漏,非常适合工业和家庭应用。 在该系统中,液化石油气(LPG)/管道天然气(PNG)泄漏的信息可通过内置 Wi-Fi...
Schematic symbols, PCB footprints, and 3D CAD models from SamacSys can be found by clicking on products in the Product Options table. If a symbol or model isn't available, it can be requested directly from the website.
Matter is single unified IP-based protocol to securely and robustly connect smart devices with each other, regardless of brand, and across smart home ecosystems.
博客 | 2024年4月15日 | ||
新闻 | 2023年1月5日 |