Robotic Lawn Mower Blog

Lawn Maintenance Getting You Down? Robotic Mowers to the Rescue!

Compared to conventional lawn mowers, robotic lawn mowers offer many benefits including they are better for our environment and offer the convenience of remote programming, controlling and monitoring.

Easy-to-Start Automotive MCU Accelerates the Development Cycle

ETS (易于入门)汽车芯片有效加速开发周期

Axel 介绍了易于使用、易于开发且易于读写的易于入门汽车芯片(ETS MCU),适用于汽车,工业,和消费类应用。

Outdoor Air Quality: It’s Not Just About Urban Areas Blog

Outdoor Air Quality: It’s Not Just About Urban Areas

Learn about the importance of air quality to our health and the benefits of being able to monitor air quality, regardless of location, with Renesas’ ZMOD4510 outdoor air quality sensor.

No Porting Required! Real-Time OS Program Development that Even a Super Beginner Can Do Blog

无需移植!即使是超级初学者也能完成的实时操作系统程序开发。

介绍实时系统项目创建功能,对于使用嵌入式实时系统的人来说,这是不可缺少的必备功能。

Ethernet TSN Switch IP Core Evaluated by Conformance Testing Provided by Spirent Communications Blog

Ethernet TSN Switch IP Core Evaluated by Conformance Testing Provided by Spirent Communications

Ethernet TSN Switch IP Core is a high-quality IP core that has passed the conformance test provided by Spirent Communications; watch the video of the IP core evaluated by FPGA using Spirent Automotive C1.

A Tiny RX23E-A Board for Digital Load Cell Blog

用于数字称重传感器的微型 RX23E-A 板

RX23E-A 在单个芯片上集成了 MCU 和高精度模拟前端 (AFE),非常适合小型化电路板以及在同一外壳中实现数字称重传感器的信号采集和信号调节。

Condition Monitoring ASICs Extend Systems’ Lifetime Blog

Condition Monitoring ASICs Extend Systems’ Lifetime

With an ASIC solution, all the condition monitoring circuitry can be placed on the same chip with all the required electronics for the core function of the product.

The Art of Networking (Series 2): PCIe Goes Automotive Blog

The Art of Networking (Series 2): PCIe Goes Automotive

In this blog, we give a brief background summary of PCIe, what its potential PCIe use cases are and what needs to be looked at to smoothen the adaption path of PCIe in future automotive applications.

Easy Azure IoT Connection! RX65N 32-bit MCU Supports Azure RTOS Blog

轻松的Azure IoT连接!RX65N 32位MCU支持Azure RTOS-

RX系列提供具有Azure认证设备认证,示例代码和用于部署Azure RTOS的IDE的评估套件。这些功能使您可以轻松连接到Azure IoT中心。