R-Car/Boards/S4SK/Yocto-Linux/SDK-v3.16.2
< R-Car | Boards/S4SK | Yocto-Linux(Redirected from R-Car/Boards/S4SK/Yocto-Linux)
|
Software revisions
Software | Revision |
---|---|
R-Car SDK | v3.16.2 |
R-Car S4 Linux Yocto package | Version 5.24.1 |
Yocto Project | 3.1.11 |
aarch64-poky-linux-gcc (GCC) | 9.3 |
Linux Kernel | 5.10.41 |
Userland 64/32bit | 64 |
U-Boot | 2020.10 |
Host PC
Ubuntu 20.04 LTS (64bit) is recommended as OS. 32bit version is not supported.
Building the BSP for R-Car S4 Starter Kit
Warning! Yocto builds require a lot of disk space (up to 100 GB). Make sure you have got enough before starting the build.
Installation of required tools and libraries
Ubuntu is used as Linux Host PC since Yocto Project Quick Start specifies Ubuntu as one of the distributions. You need to install the required packages as follows.
sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib \ build-essential chrpath socat cpio python3 python3-pip python3-pexpect \ xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa \ libsdl1.2-dev pylint3 xterm libarchive-zip-perl
Using build script
- Build script(build.sh)
#!/bin/bash POKY_COMMIT=74b22db6879b388d700f61e08cb3f239cf940d18 META_OE_COMMIT=814eec96c2a29172da57a425a3609f8b6fcc6afe META_RENESAS_COMMIT=92ddfebae62b78a65ee430d49b710bb16b719bf2 mkdir build cd build export WORK=`pwd` cd ${WORK} # Clone basic Yocto layers in parallel git clone git://git.yoctoproject.org/poky & git clone git://git.openembedded.org/meta-openembedded & git clone https://github.com/renesas-rcar/meta-renesas & # Wait for all clone operations wait # Switch to proper branches/commits cd ${WORK}/poky git checkout -b tmp ${POKY_COMMIT} cd ${WORK}/meta-openembedded git checkout -b tmp ${META_OE_COMMIT} cd ${WORK}/meta-renesas git checkout -b tmp ${META_RENESAS_COMMIT} cd ${WORK} source poky/oe-init-build-env ${WORK}/build-s4sk-gateway cp $WORK/meta-renesas/meta-rcar-gateway/docs/sample/conf/s4sk/poky-gcc/bsp/*.conf ./conf/ bitbake rcar-image-gateway
- build
./build.sh
Manual steps
- Create a directory and switch to it
mkdir build cd build export WORK=`pwd`
- Clone basic Yocto layers:
cd $WORK git clone git://git.yoctoproject.org/poky git clone git://git.openembedded.org/meta-openembedded git clone https://github.com/renesas-rcar/meta-renesas
- Switch to proper branches/commits
cd $WORK/poky git checkout -b tmp 74b22db6879b388d700f61e08cb3f239cf940d18 cd $WORK/meta-openembedded git checkout -b tmp 814eec96c2a29172da57a425a3609f8b6fcc6afe cd $WORK/meta-renesas git checkout -b tmp 92ddfebae62b78a65ee430d49b710bb16b719bf2
- Setup build environment
cd $WORK source poky/oe-init-build-env $WORK/build-s4sk-gateway
- Prepare default configuration files.
cp $WORK/meta-renesas/meta-rcar-gateway/docs/sample/conf/s4sk/poky-gcc/bsp/*.conf ./conf/
- Start the build
bitbake rcar-image-gateway
- Building image can take up to a few hours depending on your host system performance.
After the build has been completed successfully, you should see the output similar to:NOTE: Tasks Summary: Attempted 5076 tasks of which 5 didn't need to be rerun and all succeeded.
- and the command prompt should return.
Generated images
- Bitbake has generated all the necessary files in ./tmp/deploy/images directory.
You can verify its content: $ ls -1 `find ./tmp/deploy/images/s4sk/ -maxdepth 1 -type l -print` ./tmp/deploy/images/s4sk/Image ./tmp/deploy/images/s4sk/Image-s4sk.bin ./tmp/deploy/images/s4sk/modules-s4sk.tgz ./tmp/deploy/images/s4sk/r8a779f0-s4sk-s4sk.dtb ./tmp/deploy/images/s4sk/r8a779f0-s4sk.dtb ./tmp/deploy/images/s4sk/rcar-image-gateway-s4sk.manifest ./tmp/deploy/images/s4sk/rcar-image-gateway-s4sk.tar.bz2 ./tmp/deploy/images/s4sk/rcar-image-gateway-s4sk.testdata.json ./tmp/deploy/images/s4sk/u-boot-elf-s4sk.srec ./tmp/deploy/images/s4sk/u-boot-elf.srec ./tmp/deploy/images/s4sk/u-boot-initial-env ./tmp/deploy/images/s4sk/u-boot-initial-env-s4sk ./tmp/deploy/images/s4sk/u-boot-s4sk.bin ./tmp/deploy/images/s4sk/u-boot.bin
- Image is a Kernel image, *.dtb is a blob file, rcar-image-gateway-s4sk.tar.bz2 is the rootfs.
$ ls -1 tmp/deploy/images/s4sk/*.srec tmp/deploy/images/s4sk/bl31-s4sk.srec tmp/deploy/images/s4sk/tee-s4sk.srec tmp/deploy/images/s4sk/u-boot-elf-s4sk-v2020.10+gitAUTOINC+616f05eb5a-r0.srec tmp/deploy/images/s4sk/u-boot-elf-s4sk.srec tmp/deploy/images/s4sk/u-boot-elf.srec
- The built Image directory is below.
- https://hydrochoerus.com/rcar/s4sk/build/build-s4sk-gateway/tmp/deploy/images/s4sk/
- The built directory is below.
- https://hydrochoerus.com/rcar/s4sk/
How to flash/update the loader
- Write the generated bl31-s4sk.srec, tee-s4sk.srec and u-boot-elf-s4sk.srec binaries and ICUMX loader[*] to flash
- See : R-Car/Boards/S4SK#How_to_flash.2Fupdate_the_loader
- [*] Download from here
How to boot
Micro SD boot
WARNING! These steps will erase the Micro SD card completely. In short, all files will be lost.
In order to prepare you Micro SD card, follow these instructions on host machine:
- Partion your Micro SD card to set 1 partition and ID=83 (Linux)
- Make sure the Micro SD card doesn't contain any important files.
$ fdisk /dev/mmcblk0 or /dev/sdb etc. -> d -> n -> p -> 1 -> t -> 83
- Format this partition to ext4
$ mkfs.ext4 /dev/mmcblk0p1
- Mount this partition on your host to any directory and upack the rcar-image-gateway-s4sk.tar.bz2 into mounted folder.
$ mount /dev/mmcblk0p1 /mnt $ cd <your_yocto_build_directory> $ tar xjf ${WORK}/build-s4sk-gateway/tmp/deploy/images/s4sk/rcar-image-gateway-s4sk.tar.bz2 -C /mnt $ sync $ umount /mnt
- NOTE: probably you need to be a root user, hence use "sudo"
- Image and r8a779f0-s4sk.dtb are deployed under /mnt/boot/ directory
- Insert Micro SD card to S4 SK Mciro SD card slot(CN5)
- Set SW3
- SW3.1 : On
- SW3.2 : On
- SW3.3 : Off
- SW3.4 : On
- SW3.5 : Off
- SW3.6 : On
- SW3.7 : Off
- SW3.8 : Off
- SW3.1 : On
- Power ON (SW5)
Ex) => setenv bootargs rw root=/dev/mmcblk0p1 rootwait ignore_loglevel cma=560M => ext4load mmc 0 0x48080000 /boot/Image; ext4load mmc 0 0x48000000 /boot/r8a779f0-s4sk.dtb; booti 0x48080000 - 0x48000000
NFS boot
- Install some packages for NFS boot on Host PC (See R-Car/Boards/Yocto-Gen3/v5.9.0#Loading_kernel_via_TFTP_and_rootfs_via_NFS)
- Decompress the rootfs on Host PC
$ tar xjf ${WORK}/build-s4sk-gateway/tmp/deploy/images/s4sk/rcar-image-gateway-s4sk.tar.bz2 -C ${NFS_ROOT}
- Image and r8a779f0-s4sk.dtb are deployed under /mnt/boot/ directory
- Connect the Host PC to the S4SK IC101(TSN0) connector with a LAN cable
- Set SW3
- SW3.1 : On
- SW3.2 : On
- SW3.3 : Off
- SW3.4 : On
- SW3.5 : Off
- SW3.6 : On
- SW3.7 : Off
- SW3.8 : Off
- SW3.1 : On
- Power ON (SW5)
Ex) => setenv ethaddr xx:xx:xx:xx:xx:xx <- MAC address [*] => setenv ipaddr 192.168.1.3 => setenv serverip 192.168.1.2 => setenv bootargs rw root=/dev/nfs nfsroot=192.168.1.2:/srv/tftp/s4/rootfs,nfsvers=3 ip=192.168.1.3:::::tsn0 ignore_loglevel cma=560M => setenv bootcmd 'tftp 0x48080000 {Your path}/boot/Image; tftp 0x48000000 {Your path}/boot/r8a779f0-s4sk.dtb; booti 0x48080000 - 0x48000000' => saveenv Saving Environment to SPIFlash... Erasing SPI flash...Writing to SPI flash...done OK => run bootcmd Using ethernet@e68c0000 device TFTP from server 192.168.1.2; our IP address is 192.168.1.2 Filename '{Your path}/boot/Image'. Load address: 0x48080000 Loading: ########################################################## ###################### (snip) 8.7 MiB/s done Bytes transferred = 33714688 (2027200 hex) Using ethernet@e68c0000 device TFTP from server 192.168.1.2; our IP address is 192.168.1.3 Filename '{Your path}/boot/r8a779f0-s4sk.dtb'. Load address: 0x48000000 Loading: #### 6.6 MiB/s done Bytes transferred = 55591 (d927 hex) Moving Image from 0x48080000 to 0x48200000, end=4a2b0000 ## Flattened Device Tree blob at 48000000 Booting using the fdt blob at 0x48000000 Loading Device Tree to 0000000057fef000, end 0000000057fff926 ... OK Starting kernel ...
- [*]
- Check the MAC address of the board using S4_StarterKit_Configurator.exe. See R-Car/Boards/S4SK#Tab_of_S4_Starter_Kit.
- Please use the MAC address of TSN0
How to test some capabilities
Micro SD (CN5)
root@s4sk:~# dmesg|grep mmcblk
[ 0.000000] Kernel command line: rw root=/dev/mmcblk0p1 rootwait ignore_loglevel cma=560M
[ 1.934976] Waiting for root device /dev/mmcblk0p1...
[ 1.984307] mmcblk0: mmc0:aaaa SL08G 7.40 GiB
[ 1.988193] mmcblk0: p1
[ 2.223505] EXT4-fs (mmcblk0p1): recovery complete
[ 2.225750] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Opts: (null)
[ 3.806413] EXT4-fs (mmcblk0p1): re-mounted. Opts: (null)
root@s4sk:~#
root@s4sk:~# mount /dev/mmcblk0p1 /mnt/
TSN0/1 (IC101/IC104)
Ex)
root@s4sk:~# ifconfig tsn0 192.168.10.100
[ 743.368014] rswitch_get_phy_node PHY interface = sgmii
[ 744.372046] libphy: rswitch_mii: probed
[ 744.419085] mv88x2110 etha0:01: Firmware version 8.5.0.0
[ 744.455718] mv88x2110 etha0:01: attached PHY driver [mv88x2110] (mii_bus:phy_addr=etha0:01, irq=POLL)
[ 747.601932] renesas_eth_sw e68c0000.ethernet tsn0: Link is Up - 1Gbps/Full - flow control off
[ 747.603126] IPv6: ADDRCONF(NETDEV_CHANGE): tsn0: link becomes ready
root@s4sk:~# ping 192.168.10.116
PING 192.168.10.116 (192.168.10.116): 56 data bytes
64 bytes from 192.168.10.116: seq=0 ttl=128 time=0.904 ms
64 bytes from 192.168.10.116: seq=1 ttl=128 time=0.639 ms
64 bytes from 192.168.10.116: seq=2 ttl=128 time=0.854 ms
UFS
root@s4sk:~# fdisk /dev/sda
Welcome to fdisk (util-linux 2.35.1).
Changes will remain in memory only, until you decide to write them.
Be careful before using the write command.
[ 2889.819979] sda:
Command (m for help): n
Partition number (1-128, default 1): 1
First sector (256-31256570, default 256): 256
Last sector, +/-sectors or +/-size{K,M,G,T,P} (256-31256570, default 31256570): +64G
Created a new partition 1 of type 'Linux filesystem' and of size 64 GiB.
Command (m for help): w
The partition table has been altered.
Calling ioctl() to re-read partition table.
[ 2917.736661] sda: sda1
Syncing disks.
root@s4sk:~# mkfs.ext4 /dev/sda1
mke2fs 1.45.4 (23-Sep-2019)
Discarding device blocks: done
Creating filesystem with 16777216 4k blocks and 4194304 inodes
Filesystem UUID: bdf0481e-52a8-4562-a60c-24721db2ed66
Superblock backups stored on blocks:
32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632, 2654208,
4096000, 7962624, 11239424
Allocating group tables: done
Writing inode tables: done
Creating journal (131072 blocks): done
Writing superblocks and filesystem accounting information: done
root@s4sk:~# mount /dev/sda1 /mnt/
[ 2940.602149] EXT4-fs (sda1): mounted filesystem with ordered data mode. Opts: (null)
root@s4sk:~#
PCIe
PCIe Root Complex(CN30) : SSD
Environment:
- 1) MZVPV512HDGL-0000
- 2) U.2 to M.2 M-Key NVME SSD and PCIe
- 3) Oculink to U.2 Cable
- 4) SATA/IDE AC Adoperq(Japanese site)
root@s4sk:~# mount /dev/nvme0n1p1 /mnt/ [ 41.822014] EXT4-fs (nvme0n1p1): mounted filesystem with ordered data mode. Opts: (null) root@s4sk:~# mount -t tmpfs -o size=400M tmpfs /tmp root@s4sk:~# dd if=/dev/urandom of=/tmp/file bs=1M count=350 350+0 records in 350+0 records out 367001600 bytes (367 MB, 350 MiB) copied, 4.96337 s, 73.9 MB/s root@s4sk:~# cp /tmp/file /mnt/ root@s4sk:~# cp /tmp/file /mnt/ root@s4sk:~# cmp /mnt/file /tmp/file root@s4sk:~#
PCIe Root Complex(CN30) : LAN card
Environment:
- PCI-e Network Card
root@s4sk:~# dmesg|grep e1000e [ 0.977043] e1000e: Intel(R) PRO/1000 Network Driver [ 0.977678] e1000e: Copyright(c) 1999 - 2015 Intel Corporation. [ 0.986786] e1000e 0000:01:00.0: enabling device (0000 -> 0002) [ 1.025259] e1000e 0000:01:00.0: Interrupt Throttling Rate (ints/sec) set to dynamic conservative mode [ 1.088330] e1000e 0000:01:00.0 0000:01:00.0 (uninitialized): registered PHC clock [ 1.143115] e1000e 0000:01:00.0 eth0: (PCI Express:2.5GT/s:Width x1) 68:05:ca:30:bf:05 [ 1.144182] e1000e 0000:01:00.0 eth0: Intel(R) PRO/1000 Network Connection [ 1.145073] e1000e 0000:01:00.0 eth0: MAC: 3, PHY: 8, PBA No: E46981-008 [ 5.370228] e1000e 0000:01:00.0 enp1s0: renamed from eth0 root@s4sk:~# root@s4sk:~# ifconfig enp1s0 192.168.10.100 root@s4sk:~# ping 192.168.10.101 PING 192.168.10.101 (192.168.10.101): 56 data bytes 64 bytes from 192.168.10.101: seq=0 ttl=128 time=1.095 ms 64 bytes from 192.168.10.101: seq=1 ttl=128 time=1.397 ms
PCIe Endpoint(CN31)
pcitest [S4SK - Another S4 SK] :
- 1) Environments
- S4 SK board [A] : PCIe CH0(CN30)[*1] <--- OCuLink cable[*2] ---> Another S4 SK board [B] : PCIe CH1(CN31)[*3]
- [*1] PCIe CH0(CN30) : Root Complex
- [*2] Ex) https://store.supermicro.com/supermicro-55cm-oculink-to-oculink-cable-cbl-sast-0818.html
- [*3] PCIe CH1(CN31) : Endpoint
- 2) Create DTB file for Endpoint of S4 SK board [B]
- Disable: Root Complex of PCIe CH0
- Enable : Endpoint of PCIe CH1
Ex) $ cd (Your SDK Build directory) $ ls build-s4sk-gateway build_yocto.sh meta-openembedded meta-renesas poky $ source poky/oe-init-build-env build-s4sk-gateway/ $ bitbake -c devshell linux-renesas $ vi arch/arm64/boot/dts/renesas/r8a779f0-s4sk.dts (snip) &pciec0 { status = "disabled"; <-- Change to disable !!! pinctrl-0 = <&pcie0_pins>; pinctrl-names = "default"; clkreq-gpios = <&gpio2 15 GPIO_ACTIVE_LOW>; }; &pciec1_ep { status = "okay"; <-- Change to enable !!! pinctrl-0 = <&pcie1_pins>; pinctrl-names = "default"; clkreq-gpios = <&gpio2 16 GPIO_ACTIVE_LOW>; }; $ make dtbs $ exit
- Output: tmp/work/s4sk-poky-linux/linux-renesas/5.10.41+xxxxx/linux-s4sk-standard-build/arch/arm64/boot/dts/renesas/r8a779f0-s4sk.dtb
- 3) Create Image file for Endpoint of S4 SK board [B]
- Enable CONFIG_PCI_EPF_TEST and CONFIG_PCIE_RENESAS_EP
Ex) $ cd (Your SDK Build directory) $ source poky/oe-init-build-env build-s4sk-gateway/ $ bitbake -c devshell linux-renesas $ make menuconfig Device Drivers ---> [*] PCI support PCI Endpoint ---> [*] PCI Endpoint Support [*] PCI Endpoint Test driver <-- Change to "*" Device Drivers ---> [*]PCI support ---> PCI controller drivers ---> DesignWare PCI Core Support ---> [*] Renesas R-Car PCIe 4.0 Endpoint controller <-- Change to "*" $ make Image $ exit
- Output: tmp/work/s4sk-poky-linux/linux-renesas/5.10.41+xxxxx/linux-s4sk-standard-build/arch/arm64/boot/Image
- 4) Copty to binaries to Micro SD card for S4 SK board [B]
Ex) $ mount /dev/mmcblk0p1 /mnt $ cp r8a779f0-s4sk.dtb /mnt/boot/r8a779f0-s4sk_pcie1ep.dtb $ cp Image /mnt/boot/Image_ep $ ls /mnt/boot Image Image_ep r8a779f0-s4sk_pcie1ep.dtb Image-5.10.41-yocto-standard r8a779f0-s4sk.dtb
- 5) pcitest
- Step 1: Start S4 SK board [B] of Endpoint using Image_ep and r8a779f0-s4sk_pcie1ep.dtb
=> setenv bootargs console=ttySC0,921600 rw root=/dev/mmcblk0p1 rootwait cma=560M => ext4load mmc 0:1 0x48080000 /boot/Image_ep;ext4load mmc 0:1 0x48000000 /boot/r8a779f0-s4sk_pcie1ep.dtb;booti 0x48080000 - 0x48000000 (snip) s4sk login: root root@s4sk:~# sed -e 's/e65d0000.pciec0_ep/e65d8000.pciec1_ep/' ep_setup.sh > ep1_setup.sh root@s4sk:~# chmod +x ep1_setup.sh root@s4sk:~# ./ep1_setup.sh Endpoint setup mount: /sys/kernel/config: none already mounted or mount point busy. completed. root@s4sk:~#
- Step 2: Start S4 SK board [A] of Root Complex (after Step 1)
=> setenv bootargs console=ttySC0,921600 rw root=/dev/mmcblk0p1 rootwait cma=560M => ext4load mmc 0:1 0x48080000 /boot/Image;ext4load mmc 0:1 0x48000000 /boot/r8a779f0-s4sk.dtb;booti 0x48080000 - 0x48000000 (snip) s4sk login: root root@s4sk:~# sed -e 's/1024000/102400/' -e 's/1024001/102401/' pcitest_script.sh > pcitest_script_s4sk.sh root@s4sk:~# chmod +x pcitest_script_s4sk.sh root@s4sk:~# ./pcitest_script_s4sk.sh
- Log: Root Complex (S4 SK board [A])
root@s4sk:~# ./pcitest_script_s4sk.sh BAR tests BAR0: OKAY BAR4: OKAY MSI Interrupt tests SET IRQ TYPE TO MSI: OKAY MSI1: OKAY MSI2: OKAY (snip) Copy Tests COPY ( 1 bytes): OKAY COPY ( 1024 bytes): OKAY COPY ( 1025 bytes): OKAY COPY ( 102400 bytes): OKAY COPY ( 102401 bytes): OKAY root@s4sk:~#
- Log: Endpoint S4 SK board [B]
[ 44.917496] WRITE => Size: 1 bytes DMA: NO Time: 0.000001320 seconds Rate: 739 KB/s [ 45.941519] [ 45.941519] WRITE => Size: 1024 bytes DMA: NO Time: 0.000003060 seconds Rate: 326797 KB/s (snip) [ 642.777482] COPY => Size: 1 bytes DMA: NO Time: 0.000002160 seconds Rate: 452 KB/s [ 643.793517] [ 643.793517] COPY => Size: 1024 bytes DMA: NO Time: 0.000060420 seconds Rate: 16550 KB/s [ 644.809523] [ 644.809523] COPY => Size: 1025 bytes DMA: NO Time: 0.000061500 seconds Rate: 16276 KB/s [ 645.831665] [ 645.831665] COPY => Size: 102400 bytes DMA: NO Time: 0.006186660 seconds Rate: 16163 KB/s [ 646.851668] [ 646.851668] COPY => Size: 102401 bytes DMA: NO Time: 0.006195241 seconds Rate: 16141 KB/s
Thermal
root@s4sk:~# cat /sys/class/thermal/thermal_zone*/temp
39500
37500
37500
root@s4sk:~#
CPU Hotplug
root@s4sk:~# cat /sys/devices/system/cpu/online
0-7
root@s4sk:~# echo 0 > /sys/devices/system/cpu/cpu1/online
[ 145.337609] IRQ227: set affinity failed(-22).
[ 145.337764] CPU1: shutdown
[ 145.338704] psci: CPU1 killed (polled 0 ms)
root@s4sk:~# cat /sys/devices/system/cpu/offline
1
root@s4sk:~# echo 1 > /sys/devices/system/cpu/cpu1/online
[ 169.401119] Detected VIPT I-cache on CPU1
[ 169.401189] GICv3: raw_spin_lock_init for SGI
[ 169.401202] GICv3: CPU1: found redistributor 100 region 0:0x00000000f1080000
[ 169.401303] CPU1: Booted secondary processor 0x0000000100 [0x412fd050]
root@s4sk:~# cat /sys/devices/system/cpu/offline
root@s4sk:~#
Known issues & Restrictions
- [Known issue] Bitbake error messages when building SDK first time
ERROR: When reparsing <build directory>../poky/meta/recipes-core/meta/meta-environment.bb:do_generate_content, the basehash value changed from 64c5dd461f406265715a6af027a37e78b6ea72e63aa576426a354b4becee57fc to af14637c6b64b6b26c9a37492a361cc15a15be8f5ffa7ceb06618ce994035e75. The metadata is not deterministic and this needs to be fixed. ERROR: The following commands may help: ERROR: $ bitbake meta-environment-s4sk -cdo_generate_content -Snone ERROR: Then: ERROR: $ bitbake meta-environment-s4sk -cdo_generate_content -Sprintdiff
- These error message are Poky 3.1.11 bug, it doesn't affect to build output.
- Ignore error messages.
- [Restriction] The "reboot" command is not completed. Therefore, press the power(SW5) or reset(SW4) button.
Q&A site
If you have any questions, feel free to post them here.
https://community.renesas.com/automotive/gateway/
FAQ site
- https://en-support.renesas.com/knowledgeBase/category/31891 (English page)
- https://ja-support.renesas.com/knowledgeBase/category/31892 (Japanese page)