Renesas RH850 Series Contributes to the Realization of a Flying Motorcycle
A science fiction-like world in which motorcycles fly is a reality! Renesas' semiconductors for automotive applications will open up the future of mobility.
A science fiction-like world in which motorcycles fly is a reality! Renesas' semiconductors for automotive applications will open up the future of mobility.
本篇博客介绍了使用RX13T吊扇逆变器板实现连续电流PFC控制(载波频率50KHz)、无传感器矢量控制(FOC)和拾音控制的解决方案。
The RZ/G2L MPU, which integrates Arm Cortex-A55 and Cortex-M33, reduces total BOM cost by reducing the number of components and helps to mitigate procurement risk of IC components.
The ultra-low jitter ClockMatrix 2 eliminates the need for additional jitter attenuators for high-speed interfaces and supports multiple standards and protocols including Sync-E and IEEE 1588.
Renesas’ IO-Link Slave Sensor Solution showcases two examples of a resistor bridge type sensors with two different slave PHY that can be used depending on users’ system requirements.
The advanced debugging capabilities available on RA microcontroller kits provide the flexibility and convenience to debug the code quickly, easily and cost-effectively.
In this article, I will introduce the solution to the biggest challenge in AI inference, heat generation, which you have already faced or will face.
10 多年前,瑞萨做出了一个大胆的决定,推出 自主专利的 32 位 MCU——RX(Renesas Xtreme)。10 多年后的今天,我们仍然在这里并自豪地为我们的许多忠诚和满意的客户提供服务。该博客展示了自RX推出以来一直与我们在一起(使用 RX)的真正满意的客户。
Take the guesswork out of your innovation experience by following a systematic and methodical approach to start developing with Renesas RA microcontroller innovation kits.
Designers of high voltage, multi-module batteries and the systems that use them can streamline their design and development with integrated battery front end ICs and elegant daisy chaining to address higher voltages.