瑞萨电子可提供先进的器件,为工业控制、网络与计算应用实现高效可靠的通信。 我们是串行交换器件的行业领导者,可提供先进的 PCI Express® 交换机与串行 RapidIO® 交换机,并且针对最为严苛的应用情境进行了优化。 瑞萨电子是一家专为交换、桥接、信号完整性、闪存控制与计时提供 PCIe 解决方案的“一站式”供应商。 瑞萨电子也是全球知名的串行 RapidIO 交换机与桥接器供应商。 此外,我们还支持 PCI、PCI-X 与 VME 等传统总线规格。
瑞萨电子还可提供双协议收发器、电平转换器、I2C 缓冲器、工作电压范围广泛的 RS-232 收发器与 RS-485/RS-422 器件。此类器件采用小型封装,具有最高级别的抗噪能力与 ESD 保护能力,可支持高速数据传输与各种配置,从而满足您的应用需求。
IDT's RapidIO 10xN (Gen 3) compliant devices offer up to 50Gbps port speeds and 600Gbps non-blocking aggregate bandwidth and are backward compatible with previous generations. At 100ns latency, these switches offer performance to support 4G LTE-Advanced and 5G mobile infrastructure and real-time mobile edge & high performance computing. With superior energy efficiency and fault tolerance the RXS family is also well suited for imaging, aerospace, industrial control, and defense applications. The new family is composed of the RXS2448, with 24 ports and 48 lanes, and the RXS1632, with 16 ports and 32 lanes.
Presented by Trevor Hiatt, Principal Product Manager, Integrated Device Technology, Inc. Learn more at http://www.idt.com/go/rapidIO.
TRANSCRIPT
Hi. I'm Trevor Hiatt, and I'm happy to introduce IDT's next generation RapidIO switches, the RXS family. Supporting the latest 10xN RapidIO standard, these chips are extremely low latency and high bandwidth, and are designed to take on the challenges of the coming 5G mobile network, as well as other compute intensive applications. IDT introduced our prior generation of RapidIO switches in 2010, and since then they've become ubiquitous in communications infrastructure, with virtually every 4G phone call and download around the world going through our chips.
They're also being used for mobile edge and high-performance computing and data analytics. That's because RapidIO delivers the ultra-low latency needed to efficiently move and manage vast volumes of data. With our new family of RapidIO switches, ultra-fast just got a whole lot faster. We're talking about port to port latency approaching 100 nanoseconds, and a flexible non-blocking fabric with switching performance of 600 gigabits per second. That's greater than twice the performance of the prior generation, exceeding the bandwidth requirements of the 10xN standard, and all with better energy efficiency than our prior generation and competing solutions.
In addition to being optimized for 5G infrastructure, the 10xN switches are ideal for 4G LTE-Advanced systems, as well as a wide variety of markets where latency creates a bottleneck to achieving the potential performance of a system. These markets include mobile infrastructure, data center, aerospace, industrial control, and defense. The new family is comprised of the RXS2448, with 24 ports and 48 lanes, and the RXS1632 with 16 ports and 32 lanes. They're backward compatible with existing RapidIO ecosystems, protecting previous hardware and software investments. Leveraging this compatibility can accelerate a product's time to market.
There's lots more information about the RXS switches on the IDT website at www.idt.com/go/rapidio. Thanks for watching.
博客 | 2023年10月31日 | ||
博客 | 2023年7月24日 | ||
博客 | 2023年7月21日 | ||
博客 | 2023年4月3日 | ||
博客 | 2023年2月25日 | ||
博客 | 2023年2月16日 | ||
博客 | 2023年1月23日 |