Medium One, Inc.

类别: Cloud Connection , Development

Demonstrates embedded sensor connectivity and data transfer that can be monitored in real-time on the Renesas IoT Sandbox web interface.

Details

This demo uses the Synergy SK-S7G2 Starter Kit, a proximity sensor, and the AE-Wi-Fi to illustrate:

  • Real-time data transfer from a proximity sensor to a cloud platform for analytics
  • Interactive LCD display of cloud analytics, built with GUIX™ 
  • Unified onboarding and provisioning for both Ethernet and Wi-Fi (GT202)

A proximity sensor connected to the Synergy SK-S7G2 kit is used to detect the presence of a person within a specified distance. It tracks the distance, duration of presence, and the total number of detected events. The sensor sends that data to the Renesas IoT Sandbox web interface and displays it real-time on the QVGA color LCD.

Copyright Disclaimer

© 2017 Medium One. All Rights Reserved.

 

The content included herein has been provided by other companies and Renesas does not claim any ownership therein. Renesas may or may not moderate or pre-screen the content included herein. Renesas requires partners to verify the functionality of their products on Synergy Platform and Renesas is not responsible in any way for the content included herein nor its quality. Renesas does not endorse any content included herein or any opinion, recommendation, or advice expressed therein, and Renesas expressly disclaims any and all liability in connection with such content, whether or not arising under the laws of copyright, libel, privacy, obscenity, or otherwise. Renesas does not provide support for any of this content; all support requirements should be directed to the owner or licensor of the content. Renesas retains the right, at its sole discretion and without prior notice, to pre-screen, refuse, or remove any content from the Synergy Platform.

/zh/products/synergy/gallery/partner-projects/medium-one-proximity-sensor/jcr:content/gallerydownload

Download

版本 1.0.0

当前版本

发布日期: 2017-06-23

支持的MCU: S7G2

MD5: d4071a394f20cd5b64634b6b0759a0fb

下载

最新消息

N/A

安装说明

Installation instructions are provided in the accompanying application note. 

/zh/products/synergy/gallery/partner-projects/medium-one-proximity-sensor
/zh/products/synergy/gallery/partner-projects/medium-one-proximity-sensor/jcr:content/allversionsection