Digital Power Supplies for Lighting Fixtures

LED lighting product development cycles are growing shorter due to efforts to respond to new market needs. In particular, development of the power supply block, where several functions are concentrated, is a key point. One way to make development more efficient is to digitize the power supply. Digital power supplies provide three major features.

・Fewer Components

Since software can be used to tune the performance of a digital power supply, there is no need for the hardware tuning components previously required. In addition, MCUs designed for digital power supplies integrate essential peripheral functions on-chip, so the cost of external IC devices is greatly reduced.

Example of Cost Reduction by Using Digital Power Supply

Example of Cost Reduction by Using Digital Power Supply

・Shorter Development Time

It is possible to modify the operation of a digital power supply simply by making changes to the software (parameters). This means that creating a platform based on a common board and software makes it easy to derive new products from existing ones. In addition, there is a high affinity with communication functions, making it possible to develop DALI-conformant products that match market needs in a short period of time.

Differences Between Digital Power Supply and Conventional Analog Power Supply

Differences Between Digital Power Supply and Conventional Analog Power Supply

・Improved Power Supply Performance

When a sudden change in load occurs, it is possible to keep the output variation smaller with a digital configuration than with an analog one. This means that there is no longer any need for capacitors to suppress LED flicker when dimming the brightness or as a countermeasure for ripple currents. In addition, digital power supply technologies such as variable gain and auto-tuning can be used to increase responsiveness, maintain stability, and suppress variability in ways that are not possible using analog devices.

Digitizing the Power Supply for Improved Performance

Digitizing the Power Supply for Improved Performance

解决方案

LED解决方案评估系统

下面列出的硬件可用于LED照明评估,使客户能够创建与其产品相匹配的开发环境。