Renesas' radiation hardened comparators are fabricated using our dielectrically isolated radiation hardened silicon gate (RSG) process, which provides immunity to single event latch-up (SEL) and highly reliable performance in the space environment.

description文档

文档标题 language 类型 文档格式 文件大小 日期
AN9867: End of Life Derating: A Necessity or Overkill 应用文档 PDF 338 KB
Intersil Space Products Brochure 手册 PDF 3.16 MB
Intersil Commercial Lab Services 手册 PDF 364 KB

file_download下载

print新闻及更多资源

类型 日期
Rad Hard Test Reports 基本页面 2020年3月20日
Rad Hard SMD Test Flow 基本页面 2020年3月20日
Standard Data Package 基本页面 2020年3月20日
Low Dose Rate Acceptance Testing 基本页面 2020年3月26日