The Art of Networking (Series 3): The Power of Virtualization
In this blog, we describe a proof of concept (POC) where we compare the benefit of having two virtual machines (VMs) sharing an integrated hardware switch against a software switch.
In this blog, we describe a proof of concept (POC) where we compare the benefit of having two virtual machines (VMs) sharing an integrated hardware switch against a software switch.
This blog details the benefits of the Verified Linux Package which incorporates an industrial-grade Linux Civil Infrastructure Platform Super Long-term Support kernel in the RZ/G series’ Board Support Package.
Using two of our already commercially available motor evaluation kits, users can control dual motors simultaneously by changing the motor control parameters on the simple provided GUI.
在此解决方案中,您可以使用瑞萨的开发环境 对“Silex”蓝牙评估板进行无线和功耗评估。即使在开发的早期阶段,您也可以轻松获得实际的无线和电源评估数据。
The R9A06G037 CoolPhoenix 3 Powerline Modem (CPX3) has been re-certified to the PRIME Powerline standard Version 1.4 covering all security profiles as well as backward compatibility features.
完成对 Dialog Semiconductor 的收购,瑞萨电子现在可将蓝牙和 Wi-Fi 连接选项作为快速接入式物联网平台的一部分提供。
Due to the non-homogenous nature of IIoT requirements, one size does not fit all in the IIoT. ASICs offer many advantages to a customer and working with the correct supplier is key to achieving these benefits.
瑞萨电子支持 PD 和无线充电的 100W 电源适配器解决方案允许同时使用无线充电、USB-C PD 充电以及两个标准 USB 端口,使您无需在家里或办公室同时使用多个充电器。
瑞萨的智能资产跟踪标签解决方案是基于低功耗蓝牙® (LE) 的多传感器解决方案,支持数据记录、实时库存和环境数据监控,以防止记录和时间戳库存丢失和损坏。