Web Bluetooth® is a JavaScript API that works inside Chromium‑based web browsers. It's supported in Chrome and Edge browsers in Chrome OS, Windows 10, Android M+, Mac OS X, and Linux. Web Bluetooth takes advantage of the native Bluetooth hardware in your phone, Mac or PC, and facilitates interactions with peripheral devices directly from the browser. It brings some great advantages which can ease both development and product deployment using Bluetooth Low Energy.
During this webinar, we will cover:
・Web Bluetooth® - What Is It?
・Pros and Cons
・Examples of Web Bluetooth® and What It Can Do
・Demonstrate how simple Web Bluetooth® is to work with using our DA14531 Bluetooth® LE TINY
Dialog (now Renesas) offers the lowest power Wi-Fi SoC in the world. With our breakthrough low-power VirtualZero™ technology, IoT devices can now have a battery life of one year or more. This technology has the potential to replace existing low-power technologies such as Zigbee and Z Wave.
In this webinar, we explain:
・How the VirtualZero™-based DA16200 platform will disrupt the smart home market by simplifying the home architecture
・Why Wi-Fi will become the ubiquitous standard in smart homes
・What enables us to offer the lowest-power Wi-Fi SoC in the industry
The Quuppa Intelligent Locating System™ is a powerful engine for various location‑based services and applications. It provides accurate real‑time positioning data using Bluetooth® Low Energy technology, unique direction finding signal processing methods, and advanced proprietary algorithms. Hosted on the amazing DA14531 BLE from Dialog (now Renesas), this out‑of‑the‑box solution provides the ultimate value in battery life, system cost, and size.
During this webinar we will:
・Highlight Quuppa Intelligent Locating System™ - What is it? How does it work?
・Show the implementation details of a DA14531‑based Quuppa positioning tag
・Demonstrate how simple it is to start prototyping using the DA14531 TINY BLE click board
Three industry experts will show you how to cut the cost and complexity of IoT edge‑to‑cloud connectivity, and how to introduce best practices for secure management of your IoT networks by answering these questions, and many more:
What are the risks involved in the Internet of Things?
Why, if I’m designing an IoT product, should I add the cost and complexity of security into my devices?
How do I implement seamless security throughout the supply chain – in design, production, and in the field?
Open source. Open standards. Open platforms. These keywords describe how Renesas and OpenSynergy envision the future, by investing in open technologies to make the automotive industry more flexible and independent. The Virtual I/O Device (VIRTIO™) standard and the Automotive Grade Linux (AGL) platform are open source projects accelerating the development of new features and technologies for automotive cockpit solutions. They are on the way to serve as de facto automotive industry standards.
In this free, 60-minute webinar, Thomas Bruss (Renesas) and Isaac Trefz (OpenSynergy) will deliver a unique insight into how open source projects are creating a more independent and flexible automotive industry.
Key topics & takeaways:
• Discover how Open Standards can save future mobility stakeholders time and cost
• Learn how the AGL platform can accelerate the development of new features &technologies
• Understand the impact of the VIRTIO standard on hardware and software choice
• Find out about the Renesas OSS strategy, which simplifies VIRTIO integration
• Gain insight into OpenSynergy's VIRTIO-based Hypervisor, which runs AGL on a joint reference platform with Renesas
In this webinar, we will briefly review EFTs and the issues they can cause, and then look at how Renesas' RAA78815x transceivers have the industry's highest EFT immunity and are thus the perfect solution for EFT issues.
Find out how to develop embedded products that are adaptable to design changes directly from embedded hardware subject matter of experts from Renesas and embedded GUI experts from Crank Software. Join this webinar session to learn about the latest hardware - 64-bit general-purpose RZ/G2L MPUs and PMICs (Power Management ICs)- enhancing your embedded products’ solution. Also, experience how easy it is to develop GUI apps with the Storyboard through a live demo.
Solving the problem of security in your next IoT design has never been easier with the Cypherbridge SDKPac with TrustZone support integrated on the Renesas RA MCU product line. In this webinar, users will learn more about Cypherbridge Azure RTOS Solution Kits to check the boxes for design wins and accelerate time-to-market. As a Microsoft Cloud solution provider, Cypherbridge delivers tailored solutions from device to cloud, integrating embedded security and root of trust, driving edge node sensors and actuators, and securely connecting device telemetry to Azure IoT cloud services. Their value in the Renesas and Microsoft ecosystems includes project ready Azure RTOS SDKs, design services, and long term technical support from legacy to new product designs.
Currently, around 25 million devices exchange data via BACnet, which appeared in its first version in 1995. Now the manufacturer-independent communication standard is fit for the requirements of digitalisation with a secured communication structure based on TLS 1.3.
Manufacturers face the challenge of integrating the new structures with encrypted communication into new product series.
In this webinar, you will learn more about BACnet/SC and get an answer to the question why Renesas offers unique advantages with the RA series together with the BACnet stack powered by MBS.
In this webinar, you will learn:
• How the PMOD type 6A hardware architecture makes it simple to connect to any Renesas development kit
• How the integrated software reduces integration effort by providing software libraries and simple software APIs
• How the combined hardware and software solution of the Renesas Quick Connect system simplifies the transition from prototype to production
Designing stylish graphical user interfaces requires engineering and artistic skills, but artists aren't engineers and engineers aren't artists. Teamwork is required and GUILIANI, along with its WYSIWYG tool GSE, is designed to keep everybody happy; even management because GUILIANI helps to keep projects on time and on budget. This webinar will focus on the RA6M3 MCU, which is perfect for GUI because it has dedicated GUI features such as the 2D-Drawing-Engine from TES Electronic Solutions.
Renesas RZ/A2M High‑Speed Embedded AI‑Based Image Processing Microprocessors with Dynamically Reconfigurable Processor (DRP) technology are a perfect fit for mobile devices that feature a MIPI camera. Via the special DRP hardware accelerator built in the MCUs, the RZ/A2M can process images at incredible speeds. This webinar will demonstrate real‑time image processing on a GR‑MANGO board with Free‑RTOS packages and DRP Library.
Years of experience with smartphones has taught us to expect a fluid and intuitive user interface on a touchscreen. As touch user interfaces spread to a wider range of devices, device manufacturers are facing challenges as they struggle to deliver a smartphone-like user experience, especially in lower-cost products and markets. Nothing is more likely to break a user’s trust in a device than a touch interface whose response lags their input by too long, or which cannot react consistently to multiple touches. This webinar takes a look at how Qt on Renesas RA6 MCUs can address these concerns.