Demonstration of various components of the Express Logic Xware (ThreadX, GUIX, NetX and USBX) running on Renesas RZ/A1H. The ThreadX RTOS manages the threads, the UI is built on GUIX, the embedded system and the webpage communicate using NetX and the patient records are stored locally on the embedded system in a flash storage medium using USBX. All of these components are fine-tuned to run on the Renesas RZ/A1H microprocessor with 10MB on chip SRAM.