Application Notes of using the code generator plug-in for the RL78 (Reference links)
MCUs | Application Note | Source Code | Description |
---|---|---|---|
RL78/G10 | RL78/G10 Automatic Hand Soap Dispenser Application Notes Rev.1.00 (PDF | English, 日本語) | C source (e² studio, CS+) RL78/G10 Wi-Fi module (ESP-WROOM-02) control sample software for TCP/IP Slave Transmission/Reception Rev.1.10 (ZIP) |
This application note explains how to realize automatic hand soap dispenser using RL78/G10. |
RL78/G10 Wi-Fi module (ESP-WROOM-02) control sample software for TCP/IP Slave Transmission/Reception Rev.1.10 (PDF | English, 日本語) | C source (e² studio, CS+) RL78/G10 Wi-Fi module (ESP-WROOM-02) control sample software for TCP/IP Slave Transmission/Reception Rev.1.10 (ZIP) |
This application note describes how to use the software for controlling the Wi-Fi module ESP-WROOM-02 through the RL78/G10 and its sample application program. | |
RL78/G12 | RL78/G12 A/D Converter (Software Trigger and Sequential Conversion Modes) CC-RL Rev.1.00 (PDF | English, 日本語) | C source (e² studio, CS+) RL78/G12 A/D Converter (Software Trigger and Sequential Conversion Modes) CC-RL Rev.1.00 - Sample Code (ZIP | English, 日本語) |
This application note describes the procedures for performing A/D conversion on analog voltages using the RL78/G12's A/D converter (supporting software trigger and sequential conversion modes). |
RL78/G12 Timer Array Unit (Interval Timer) CC-RL Rev.1.10 (PDF | English, 日本語) | C source (e² studio, CS+) RL78/G12 Timer Array Unit (Interval Timer) CC-RL Rev.1.10 (ZIP | English, 日本語) |
This application note describes the interval timer function of the timer array unit (TAU). | |
RL78/G13 | RL78/G13 代码生成的应用实例(参考例程) Rev.1.00 (PDF | English, 日本語, 简体中文) | C source (e² studio) RL78/G13 代码生成的应用实例(参考例程) Rev.1.00 - Sample Code (ZIP | English, 日本語, 简体中文) |
This document describes using the sample program with the Code Generator for e² studio. The CC-RL is used as a compiler in the sample program. |
RL78/G13 A/D Converter (Software Trigger and Sequential Conversion Modes) CC-RL Rev.2.00 (PDF | English, 日本語) | C source (e² studio, CS+) RL78/G13 A/D Converter (Software Trigger and Sequential Conversion Modes) CC-RL Rev.2.00 - Sample Code (ZIP | English, 日本語) |
This application note describes the procedures for performing A/D conversion on analog voltages using the RL78/G13's A/D converter (supporting software trigger and sequential conversion modes). | |
RL78/G13 Serial Array Unit (UART Communication) CC-RL Rev.2.00 (PDF | English, 日本語) | C source (e² studio, CS+) RL78/G13 Serial Array Unit (UART Communication) CC-RL Rev.2.00 - Sample Code (ZIP | English, 日本語) |
This application note explains how to use UART communication through the serial array unit (SAU). ASCII characters transmitted from the device on the opposite side are analyzed to make responses. | |
RL78/G13 Timer Array Unit (PWM Output) CC-RL Rev.2.00 (PDF | English, 日本語) | C source (e² studio, CS+) RL78/G13 Timer Array Unit (PWM Output) CC-RL Rev.2.00 - Sample Code (ZIP | English, 日本語) |
This application note describes the PWM output function of the timer array unit (TAU). | |
RL78/G13 DMA控制器(UART连续接收) CC-RL Rev.1.00 (PDF | English, 日本語, 简体中文) | C source (e² studio, CS+) RL78/G13 DMA Controller(UART Sequential Reception) CC-RL Rev.1.00 - Sample Code (ZIP | English, 日本語) |
This application note explains how to use the RL78/G13 DMA controller for sequential reception through the UART. | |
RL78/G13 Timer Array Unit (Pulse Interval Measurement (Both edges)) CC-RL Rev.1.00 (PDF | English, 日本語) | C source (e² studio, CS+) RL78/G13 Timer Array Unit (Pulse Interval Measurement (Both edges) CC-RL Rev.2.00 - Sample Code (ZIP | English, 日本語) |
This application note describes how the timer array unit measures time intervals between pulses. | |
RL78/G13 Serial Array Unit for 3-Wire Serial I/O (Master Transmission/Reception) CC-RL Rev.2.01 (PDF | English, 日本語) | C source (e² studio, CS+) RL78/G13 Serial Array Unit for 3-Wire Serial I/O (Master Transmission/Reception) CC-RL Rev.2.01 - Sample Code (ZIP | English, 日本語) |
This application note describes how the serial array unit (SAU) performs master transmission and reception by 3-wire serial I/O communication (CSI). | |
RL78/G14 | RL78/G14 Measuring Distance to an Object with Ultrasonic Sensor CC-RL Rev.1.00 (PDF | English, 日本語) | C source (e² studio, CS+) RL78/G14 Measuring Distance to an Object with Ultrasonic Sensor CC-RL Rev.1.00 - Sample Code (ZIP) |
This application note describes an example to measure distance to an object with ultrasonic sensor. |
RL78/G14 Haptic Feedback Control by a Piezoelectric Actuator CC-RL Rev.1.00 (PDF | English, 日本語) | C source (e² studio, CS+) RL78/G14 Haptic Feedback Control by a Piezoelectric Actuator CC-RL Rev.1.00 - Sample Code (ZIP) |
This application note describes an example to drive piezoelectric haptic actuators. | |
RL78/G14 A/D转换器(软件触发、连续转换模式) CC-RL Rev.1.00 (PDF | English, 日本語, 简体中文) | C source (e² studio, CS+) RL78/G14 A/D Converter (Software Trigger and Sequential Conversion Modes) CC-RL Rev.1.00 - Sample Code (ZIP | English, 日本語) |
This application note describes the procedures for performing A/D conversion on analog voltages using the RL78/G14's A/D converter (supporting software trigger and sequential conversion modes). | |
RL78/G14 定时器阵列单元(间隔定时器)CC-RL Rev.1.00 (PDF | English, 日本語, 简体中文) | C source (e² studio, CS+) RL78/G14 Timer Array Unit (Interval Timer) CC-RL Rev.1.00 - Sample Code (ZIP | English, 日本語) |
This application note describes the interval timer function of the timer array unit (TAU). | |
RL78/L13 | RL78/L13 Low power consumption of LCD drive Using Voltage Detector (LVD) Rev.1.00 (PDF | English, 日本語) | C source (e² studio, CS+) RL78/L13 Low power consumption of LCD drive Using Voltage Detector (LVD) Rev.1.00 - Sample Code (ZIP | English, 日本語) |
This method consumes larger power than the capacitor split method does, which is a problem to be solved. |
RL78/L13 Serial Array Unit (UART Communication) CC-RL Rev.1.00 (PDF | English, 日本語) | C source (e² studio, CS+) RL78/L13 Serial Array Unit (UART Communication) CC-RL Rev.1.00 - Sample Code (ZIP | English, 日本語) |
This application note explains how to use UART communication through the serial array unit (SAU). ASCII characters transmitted from the device on the opposite side are analyzed to make responses |
A Note to Users of the Code Generator Plug-in for RX: Migrating to the Smart Configurator
We recommend that you consider migrating to the Smart Configurator, as it supports the following three functions: importing middleware in the form of FIT modules, generating driver code, and setting pins from the Code Generator Plug-in.
- Smart Configurator
- Renesas e² studio Porting projects produced with the Code Generator to projects for use with the Smart Configurator (PDF | English, 日本語)
From now on, we do not intend to add or modify the support for devices beyond that provided by the Code Generator Plug-in for RX V1.16.00. However, we will continue to support the Code Generator Plug-in for RX users. Also, if you intend to continue using the Code Generator Plug-in for RX, please refer to the release notes for instructions on usage.