图像
Christos Aslanidis
Christos Aslanidis
Manager
已发布: 2021年8月10日

The next evolutionary step for narrowband power line communication (PLC) technologies has taken place with the introduction of the “Hybrid” extension. This allows each node in the mesh network to use either PLC or RF communication depending on the best available channel and to keep maximum coverage, the selection can be adjusted dynamically. Furthermore, the hybrid specification opens new use cases besides the classical automatic meter reading, for instance, sub-metering, in-home displays, lighting controllers, and others.

To address this technology Renesas is using the well-known connectivity products CPX3 (R9A06G037) and TsuRuGi (RAA604S00).

CPX3 is Renesas’ software configurable PLC modem which supports all main PLC standards covering all global frequency bands with a single PCB design (Power Line Communication (PLC) Solutions).

TsuRuGi is the sub-GHz transceiver which in combination with the RX651 MCU supports the wireless communication profiles defined by the Wi-SUN alliance based on the international standard IEEE 802.15.4. (Sub-GHz/Wi-SUN Protocol Stack)

Both devices CPX3 and TsuRuGi are part of the “golden units” which are used for the certification in the related alliances.

Looking at the overall system architecture of Renesas’ G3-PLC hybrid solution, shown in Figure 1, it is clear to see that any end product platform can retain its flexibility and modularity and is able to extend a pure PLC product, into a hybrid one, by simply adding an RF transceiver module.

图像
Overall system architecture of Renesas’ G3-PLC hybrid solution
Figure 1

Renesas showcased this solution at Enlit Europe which took place from November 30 to December 2, 2021 in Milan, Italy.