Azure-Certified Kits Featuring both RA and RX Families of 32-bit MCUs Enable Reliable and Secure End-to-End Cloud Solutions

2023年4月6日

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced that its cellular-to-cloud development kits powered by Renesas’ 32-bit microcontrollers (MCUs) now fully support Microsoft’s popular Azure cloud services. The two Cloud Kits – the CK-RA6M5 and CK-RX65N – enable users to readily connect and manage wireless IoT devices via the cloud. With these latest updates, IoT device developers can now take advantage of unique features and services available through Azure, an open and flexible cloud computing platform used by billions of devices worldwide.

Both cloud development kits incorporate Renesas’ LTE CAT-M1 module, which wirelessly connects MCUs to cloud services without a gateway. The kits are equipped with Microsoft’s new Embedded Wireless Framework, providing a simplified link to the Azure cloud platform. The Embedded Wireless Framework lets any network adapter securely connect to the cloud, providing greater flexibility and better lifecycle management of cloud-based products. Asset tracking, building automation, medical data management, voice command and industrial control are some of the embedded applications that can benefit from the Renesas Cloud Kits.

To ensure reliable functionality and interoperability, both CK-RA6M5 and CK-RX65N kits have been certified by Microsoft Azure. This means that the devices are validated to connect with Azure IoT Hub and can be securely provisioned through the Device Provisioning Service. Additionally, both devices are IoT Plug and Play-certified, enabling developers to integrate the devices into their solutions using pre-defined device models. This eliminates the need to manually configure hardware.

The Renesas Cloud Kits include a high-performance MCU, the RYZ014A Cat-M1 Pmod, six on-board sensors, and extensive peripherals, including a USB FS connector, USB-to-UART serial converter, two PMOD connectors, and a battery connector. For additional layers of security, Renesas collaborated with its partner, Crypto Quantique to implement a software-based IoT cryptography platform that securely connects IoT devices to server-hosted applications on-premises or in the cloud. Hardware-based security such as the Renesas Secure Crypto Engine 9 (SCE9) and Trusted Secure IP (TSIP) driver has been incorporated on the RA6M5 and RX65N MCUs respectively.

"The opportunities that the Azure cloud platform brings to IoT developers are limitless,” said Roger Wendelken, Senior Vice President and Head of MCU Business in Renesas’ IoT and Infrastructure Business Unit. “Our Azure-enabled Cloud Kits provide engineers with a powerful development environment to create, evaluate and deploy cloud-based IoT solutions with confidence. With real-time data analytics and easy integration with other Azure services, developers can focus on building best-in-class IoT applications."

"Bringing the Renesas Cloud Kits into the Azure cloud ecosystem is a natural step forward,” said Stefan Wick, Product Lead IoT Edge and RTOS at Microsoft Azure. “By customizing the Embedded Wireless Framework for Renesas’ MCUs, engineers can reuse application code across different IoT products and leverage a flexible abstraction interface for seamlessly connecting IoT systems to the Azure cloud services. Using the pre-configured development platform, system developers can leverage the power of Azure IoT and create reliable and scalable IoT solutions, while saving time and cost for development.”

"We are proud to have been involved in the implementation of enhanced security measures for the Renesas Cloud Kits, as well as providing seamless and speedy connectivity to the Azure cloud,” said Chris Jones, Director of Applications at Crypto Quantique. “Our QuarkLink IoT platform provides industry-leading security, giving customers peace of mind knowing that their data and devices are secure."

Simplifying AI/ML at the Edge

Renesas’ Cloud Kits make it easy to collect data from onboard sensors, upload them to the cloud for AI/Machine Learning processing and tools, and download the model back to the end point. Simplified development software is available out-of-the-box, including Reality AI Tools and Edge Impulse Studio. Reality AI Tools provide a true endpoint AI for a range of applications, including anomaly detection and voice recognition. The Edge Impulse Studio integrated cloud environment enables end-to-end AI/ML development using the kits’ accelerometer for asset and package tracking use cases.

Winning Combination

The Renesas Cloud Kits are part of the Quick-Connect IoT Platform where developers can seamlessly connect to additional sensors or connectivity options via the standard Pmod interfaces. This enables users to easily expand their use-cases and even graphically build software with Quick-Connect Studio. Learn more about these solutions with the Cellular Cloud Connected System Winning Combination which can help accelerate time-to-market.

Renesas MCU Leadership

A world leader in MCUs, Renesas ships more than 3.5 billion units per year, with approximately 50% of shipments serving the automotive industry, and the remainder supporting industrial and Internet of Things applications as well as data center and communications infrastructure. Renesas has the broadest portfolio of 8-, 16- and 32-bit devices, and is the industry's No. 1 supplier of 16- and 32-bit MCUs combined, delivering unmatched quality and efficiency with exceptional performance. As a trusted supplier, Renesas has decades of experience designing smart, secure MCUs, backed by a dual-source production model, the industry’s most advanced MCU process technology and a vast network of more than 200 ecosystem partners. For more information about Renesas MCUs, visit: www.renesas.com/MCUs.

Availability

Both the CK-RA6M5 and CK-RX65N are available today. For more information about Renesas cloud solutions, please visit: renesas.com/cloudsolutions.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) empowers a safer, smarter and more sustainable future where technology helps make our lives easier. The leading global provider of microcontrollers, Renesas combines our expertise in embedded processing, analog, power and connectivity to deliver complete semiconductor solutions. These Winning Combinations accelerate time to market for automotive, industrial, infrastructure and IoT applications, enabling billions of connected, intelligent devices that enhance the way people work and live. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, YouTube, and Instagram.

(Remarks) All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.