- CC-RL, CC-RX, CC-RH -

Thank you for purchasing compiler products from Renesas.
This page is intended for users who have purchased licenses for the CC-RL, CC-RX, or CC-RH compilers.
Follow the steps below before using a compiler product.

1. Reading the Software License Agreement

2. Installing an IDE

3. Acquiring a license key (if you have purchased an annual license)

4. Registering the license key

5. Tool user registration (recommended)

Related user’s manuals/Individual compiler product pages

If you have purchased a compiler license and not yet received the license key (or license acquisition code), you can use the free evaluation edition of the compiler* by following steps 1 and 2 below.
After having received the license key, follow steps 3 and 4.
*The trial period of a free evaluation edition is 60 days. See for details: Evaluation software tools

 

1. Reading the Software License Agreement

Before using a compiler product (CC-RL, CC-RX, or CC-RH), carefully read the Software License Agreement at the link below.

SOFTWARE LICENSE AGREEMENT_LLWEB-20179381

 

2. Installing an IDE

【For Windows】  
(1) Installing an IDE
Download and install installer for an IDE from below.
The e² studio and CS+ are available for use as IDEs.
Executing the installer for the IDE installs the IDE along with the compiler and the license manager you intend to use.
*From July 2022, the CC-RH compiler has also been made usable with the e² studio. Combinations of CC-RH V2.04.00 and later versions and e² studio 2022-07 and later versions are supported.

Integrated Development EnvironmentDownload
e² studio
See details of e² studio
e² studio 2024-04
CS+
See details of CS+
CS+ for CC V8.11.00

(2) Installing the license management software
If you have purchased a floating license, you will need to install the license management software on a server PC.

Software for floating license management (for a server PC)

If you have already installed the required software, go to step 3.

【For Linux】        
(1) Installing a compiler       
Download and install installer for a compiler from below.

CC-RL V1.13.01 for Linux                
CC-RX V3.06.01 for Linux      
CC-RH V2.06.01 for Linux  

(2) Installing an IDE   
Download and install installer for an IDE from below.

e² studio 2024-04 for Linux

(3) Installing the license management software            
Download and install the license manager installer.
*The floting license cannot be used on Linux. (Will be available in October)

License manager V2.07.00 for Linux  

 

3. Acquiring a license key (if you have purchased an annual license)

  1. Ensure that you have the license acquisition code that came with the compiler package.
  2. Log in to My Renesas on the Renesas Web site.
    My Renesas: https://www.renesas.com/myrenesas
  3. Select [Obtain Subscription License Key] from the menu, and register the license acquisition code.

*The license key is valid for one year from the time of acquisition (initial registration of the license acquisition code).
If you purchase a new license to use a compiler for a second year, for example, we recommend only acquiring a new license key when you need to use the compiler again after the first license has expired or at the time the first license expires.

 

4. Registering the license key

If you have purchased a permanent license, make sure you have the license-key certificate that came with the compiler package.
If you have purchased an annual license, make sure you have the license key you received through step 3, Acquiring a license key.

Node-Locked License

【For Windows】
Watch this video and follow the procedure listed below. (0:25 to 1:18)

  1. Select [Renesas Electronics Utilities] from the Windows start menu (or [All Programs]) and then [Renesas License Manager].
  2. If you have an upgrade license, confirm that the [License Manager] window indicates the license to be upgraded.Note1
  3. Click on the [Add license] button. The [Add Node Locked License] window appears.
  4. Enter the license key in the [Add following License keys] field and click on the [Add] button.
  5. Check that the name of the compiler license you have purchased is displayed in the [License Manager] window.
    *When you click on the name of an annual license, the type of license (Node-Locked or Floating) and expiration date are displayed in the lower pane of the window.
  6. Click on [Quit] to close the License Manager.

【For Linux】

  1. When adding a license, enter the following in the terminal.
    $ /usr/local/renesas-mcutools/bin/license-manager --add <Licence Key>
  2. When checking registered license information, enter the following in the terminal.
    $ /usr/local/renesas-mcutools/bin/license-manager --list
  3. For other usage methods, enter the following in the terminal.
    $ /usr/local/renesas-mcutools/bin/license-manager --help
Notice of an error
When building using the Linux compiler, there is a problem that E0511182 error might occur. We apologize for the inconvenience, but until the problem is resolved, please try the solutions in the FAQ.

Floating License

Watch this video and follow the procedure listed below.
If you have an upgrade license, confirm that the license to be upgraded has already been indicated in the [Floating License Server Administrator] window.Note1

  1. Server PC: Register the license key on the floating license server. (1:11)
  2. Client PC: Start up the License Manager to make the initial settings for using a floating license. (1:42)

You can also check the above procedure in the following user’s manuals.

Floating License Server V2.04.00 User's Manual Rev.1.00 (PDF | English, 日本語)
License Manager User's Manual|2.3.6 Setting up the floating license

*The floting license cannot be used on Linux. (Will be available in October)

Note

  1. For the upgrade license that you need to confirm as that to be upgraded, refer to the following examples.
    If the license you require is not indicated, register the license to be upgraded and then register the upgrade license.

- Upgrade license for a version (Professional edition): A license for the Professional edition of the previous version of the same compiler
  Example: For CC-RX V3 Upgrade (version), confirm that a license for “Compiler Professional V2 for RX (CC-RX)” is indicated.
- Upgrade license for a version (Standard edition): A license for the Standard or Professional edition of the previous version of the same compiler
  Example: For CC-RH V2 Upgrade (version), confirm that “Compiler Standard (or Professional) V1 for RH850 (CC-RH)” is indicated.
- Upgrade license for an edition of the same version: A license for the Standard edition of the same version of the same compiler
  Example: For CC-RX V3 Upgrade (edition), confirm that “Compiler Standard V3 for RX (CC-RX)” is indicated.

 

This completes preparations for the use of a compiler product.


 

5. Tool user registration (recommended)

We recommend registration as a user for managing and preventing the loss of tool products you have purchased.

How to Register a product

  1. Click on [Software/Tool Registration] in the MyRenesas menu.
  2. On the "Software/Tools Registered" page, click on [Add].
  3. On the "Register a Software/Tool" page, enter the required information on your product (as shown in the example below) and click on [Register].
    Product category: Compiler/Assembler
    Product name (example): RX Family C/C++ Compiler Package [CC-RX]
    License key: The license key that you registered in step 4, Registering the license key

     

Related user’s manuals

Individual compiler product pages

FAQ

 


Contact

If you have any inquiries, please contact us from the following link.
Contact support