2022-08-04

The system notifies you with a change in the rotating light color when a variable matches a user-defined condition (variable + threshold condition)!

  • Multiple variables can be monitored.
  • Multiple conditions can be set for one variable.
  • Information that matches the conditions is displayed as a log on the list screen.