Overview

Detecting a face and certified person based on NEC NeoFace technology. Displaying information of authenticated person or “Unknown”.
No limitation of the number of people to authenticate but the processing speed depends on the number of people.

System Block Diagram

A face is detected from a camera image. And the registered person is specified.

System Block Diagram

Recommended Products

xxxxxxxxxxxxxxxxxxxxxxxxxxxx

Semiconductor Device Recommended Products Features, etc.
xxxxxxxxxx xxxxxxxxxx
  • xxxxxxxxxx