Smart Analog Easy Starter is a GUI evaluation tool for designing the analog front-end circuit of Smart Analog devices and editing analog circuit data while observing the waveforms on a computer screen. Circuit design can be performed easily by operating a mouse on a computer screen using a Smart Analog evaluation board manufactured by Tessera Technology.

System Configuration

Smart Analog Easy Starter 101 System Configuration

Smart Analog Easy Starter System Configuration

Main Features
  • GUI tool for Smart Analog evaluation board
  • Perform circuit design and customization using a circuit block diagram style GUI.
  • The circuit data (register values, etc.) you create can be displayed in a list, saved, and restored
  • AFE register files created in the Renesas VA online simulator can be imported*1
  • Edit circuit data while observing waveforms in Easy Starter
  • Generate C source code for circuit design*2
  • Generated C source code is compatible with files generated by SA-Designer (project not registered to CS+)

*Notes:

  1. AFE register files created in Renesas VA cannot be imported to Smart Analog Easy Starter 101.
  2. Except interface C source code.
Downloads

A My Renesas user ID and password are required to download.

*Note: 3. For evaluation boards with Smart Analog IC501/502, please inquire.

Other Files

Name
RL78/G1E Stick Hex File
Dedicated microcontroller software (hex file) that re-enables use of Smart Analog Easy Starter after the microcontroller software of the RL78/G1E mounted on the Smart Analog Stick or RL78/G1E Stick has been rewritten.
RL78/G1E Stick Phototransistor Settings
Setting file (.ini extension) for Smart Analog Easy Starter for using the RL78/G1E to configure an optimal AFE circuit for the phototransistor mounted on the Smart Analog Stick or RL78/G1E Stick.
TSA-IC300 Hall element setting file
Setting file (.ini extension) for Smart Analog Easy Starter for using the RL78/G1A and SAIC300 to configure an optimal AFE circuit for the Hall element mounted on the TSA-IC300.
TSA-IC300 USB drivers
Please download USB drivers for TSA-IC300 for Windows 7, Windows XP, and Windows Vista from Tessera Technology's website
TSA-IC300/TSA-IC301 Hex File
Dedicated microcontroller software (hex file) that re-enables use of Smart Analog Easy Starter after the microcontroller software of the RL78/G1A mounted on the TSA-IC300 (or TSA-IC301) has been rewritten.
TSA-IC301 Hall Element Settings
Setting file (.ini extension) for Smart Analog Easy Starter for using the RL78/G1A and SAIC301 to configure an optimal AFE circuit for the Hall element mounted on the TSA-IC301.
TSA-IC301 USB drivers
Please download USB drivers for TSA-IC301 for Windows 7, Windows XP, and Windows Vista from Tessera Technology's website
TSA-IC500 Phototransistor Settings
Setting file (.ini extension) for Smart Analog Easy Starter for using the RL78/G1A and SAIC500 to configure an optimal AFE circuit for the phototransistor mounted on the TSA-IC500.
TSA-IC500 USB drivers
USB drivers for TSA-IC500 and RL78/G1E-Stick for Windows 7, Windows XP, and Windows Vista
TSA-IC500 hex file
Dedicated microcontroller software (hex file) that re-enables use of Smart Analog Easy Starter after the microcontroller software of the RL78/G1A mounted on the TSA-IC500 has been rewritten.
TSA-OP-IC101 hex file
Dedicated microcontroller software (hex file) that re-enables use of Smart Analog Easy Starter after the microcontroller software of the RL78/L13 mounted on the TSA-OP-IC101 has been rewritten.
TSA-OP-IC101 thermistor setting file
Setting file (.ini extension) for Smart Analog Easy Starter for using the RL78/L13 RSK and SAIC101 to configure an optimal AFE circuit for the thermistor mounted on the TSA-OP-IC101.
Hardware Requirements
Supported OS Windows® 7, Windows Vista®, Windows® XP SP3
CPU At least 1 GHz (multicore CPU supported)
Main memory At least 1 GB
Display At least 800 x 600
Interface At least 1 USB port that supports USB 1.1
Other software requirements in addition to Windows OS Microsoft .NET Framework 3.0 USB driver for target board
Process Flow
  1. Write hex file for running Smart Analog Easy Starter (using Renesas Flash Programmer)*4
  2. Connect computer and board*5
  3. Start Smart Analog Easy Starter
    Run Start.exe
  4. Select register (default) and target board*6
    Select target board and main screen opens
  5. Design analog circuit
    Set analog circuits
  6. Observe waveforms and check A/D conversion values
    A/D conversion settings and results
  7. Check register setting values and output C source code
    Display register settings and output C source code
  8. Save analog circuit design information and read
    Save analog circuit design information
  9. Embed C source code to user program and debug

*Notes:

4. TSA-IC300/TSA-IC301, TSA-IC500, and RL78/G1E-STICK ship with hex file pre-programmed, so this process is unnecessary if you have not overwritten the program after purchasing.

5. Please install a USB driver when you connect a Smart Analog evaluation board to your computer for the first time.

6. If connecting a Smart Analog evaluation board, go to File and uncheck GUI Trial Mode.