RH850/C1M-A 入门套件
RH850/C1M-A 入门套件是一款简单易用的平台,用于评估瑞萨电子 32 位 RH850/C1M-A2 微控制器的特性和性能。
RH850/C1M-Ax 微控制器配备 RH850 系列 G3MH(C1M-A2 为双核)CPU 内核(C1M-A1 工作频率为240MHz、C1M-A2 工作频率为 320MHz),拥有出色的处理能力。 除 ROM、RAM 和 DMA 外,这款微控制器还内置多种定时器(如电机控制定时器)、多种串行接口(如 CAN,其中 CAN FD 兼容)、12 位 A/D 转换器 (ADC)、可将旋转变压器输出信号转换为数字角度信息的 R/D 转换器 (RDC3A) 、CPU 以及并行电机控制单元 (EMU3) 等,还配备有适用于 HEV/EV 电机控制的多种外围功能。 此外,C1M-A2 可以同时控制两个电机。
另有依照 NDA 发布的功能安全及信息安全文档请求链接。 请求文档
Software title
|
Software type
|
公司
|
---|---|---|
ASCET-DEVELOPER ETAS ASCET-DEVELOPER (ASCET 7) is a tool for developing application software for embedded systems using graphical models and textual programming notations.
|
Other Hardware | ETAS Group |
ETK / FETK / XETK – ECU Interfaces The Ethernet-based ETK / FETK / XETK interfaces by ETAS provide direct access to the measurement variables and control parameters of an ECU.
|
Other Hardware | ETAS Group |
INCA INCA tools are used for ECU development and test as well as for validation and calibration of electronically controlled systems in the vehicle, on the test bench, or in a virtual environment on the PC.
|
IDE and Coding Tool | ETAS Group |
E2 emulator [RTE0T00020KCE00000R] On-chip debugging emulator. Also available as a flash memory programmer. [Support MCU/MPU: RA, RE, RH850, R-Car D1, RL78, RX, RISC-V MCU]
|
Emulator | 瑞萨电子 |
Renesas Flash Programmer (Programming GUI) Flash memory programming software [Support MCU/MPU and devices: RA, RE, RX, RL78, RH850, RISC-V MCU Renesas Synergy, DA1459x, DA1469x, DA1470x, Power Management, Renesas USB Power Delivery Family, ICs for Motor Driver/Actuator Driver, V850, 78K0R, 78K0]
|
Programmer (Unit/SW) | 瑞萨电子 |
RH850 Multicore Model-Based Environment [Embedded Target for RH850 Multicore] The Embedded Target for RH850 Multicore is a RH850 model-based multicore environment that simplifies complex driving control for the autonomous-driving era. In addition to the multicore support of the PILS tool for automatic configuration of environments, Embedded Target for Renesas CS+, it can also be interlinked with a model-based parallelization tool from eSOL Co., Ltd.
|
Model-Based Development | 瑞萨电子 |
瑞萨 MCAL 瑞萨的 MCAL(微控制器抽象层)软件驱动程序可作为独立软件包获取。
|
Software Package | 瑞萨电子 |
xEV Inverter Application Model & Software An xEV (Electric Vehicle) runs on a motor or combination of motor and internal combustion engine, and the motor is controlled by the xEV Inverter. The “xEV Inverter Application Model and Software” provides a sample application model and software to control the motor, reducing software development effort and time during product development using the xEV inverter kit.
|
Software Package | 瑞萨电子 |
IAR Embedded Workbench for Renesas RH850 IAR Embedded Workbench 可为 RH850 设备提供广泛支持。 IAR Embedded Workbench 是一套具备领先优化技术的完整开发工具,可用于创建强大的汽车应用程序。
|
IDE and Coding Tool | IAR Systems |
Green Hills Multi 多开发环境:快速开发、调试、测试以及优化嵌入式应用和实时应用。Green Hills 优化编译器:使用 C、C++ 和 Ada 生成最小和最快的代码。
|
IDE and Coding Tool | Green Hills Software LLC |
RH850 Smart Configurator RH850 Smart Configurator is an automatic driver generation tool for internal peripheral I/O modules through GUI settings.
|
Solution Toolkit | 瑞萨电子 |
MBD Solution for RH850/C1M-Ax The MBD solution for RH850/C1M-Ax connects the MCU peripheral IP model with the user model through an intuitive physical value interface and realizes seamless Model-Based Design (MBD) from simulation to embedding generated code into the actual hardware.
|
Model-Based Development | 瑞萨电子 |
Green Hills MULTI Device-Support-Packages Green Hills MULTI Device-Support-Packages include all device specific files to be used with the MULTI IDE.
|
IDE and Coding Tool | 瑞萨电子 |
13 items
|
RH850/C1M-A 入门套件是一款简单易用的平台,用于评估瑞萨电子 32 位 RH850/C1M-A2 微控制器的特性和性能。
This traction motor controller mainly intends to drive motor control for HEV/EV-based applications and these consist of two boards – the controller board which controls...
车载逆变器用于将直流电流转换为交流电,该交流电用于电动汽车的电机中。该套件结合了MCU,电源管理IC,栅极驱动器IC,隔离栅极双极晶体管(IGBT)和快恢复二极管(FRD),使高性能HEV / EV电机,实用的硬件设计得到最大限度的使用。此外,还提供 xEV 逆变器应用模型和软件...
Schematic symbols, PCB footprints, and 3D CAD models from SamacSys can be found by clicking on products in the Product Options table. If a symbol or model isn't available, it can be requested directly from the website.
了解更多关于构建世界上最小的100KW级电动汽车逆变器的参考解决方案。
博客 | 2021年11月4日 | ||
博客 | 2021年7月19日 |
Analog/Power Device | Recommended Product | Features | Featured Document | Ordering |
---|---|---|---|---|
Power Management IC | RAA270000KFT | Ideal power solution for RH850/E1x/C1x. Integrated fault diagnosis and monitor functions. | RAA270000KFT Data sheet (PDF) | Contact Sales |
Gate Driver | R2A25110KSP | IGBT Gate Driver with insulating function (micro-isolator), isolation voltage: 2.5KVrms, excessive current protection function, mirror clamp function, soft turnoff function, etc. | R2A25110KSP Datasheet Rev.5.2 (PDF) | Contact Sales |