IDT to Exhibit Wireless Power Solutions at the 2014 International Consumer Electronics Show in Las Vegas, January 7-10
SAN JOSE, Calif., December 17, 2013 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that it will be exhibiting its industry-leading wireless power solutions at the 2014 International Consumer Electronics Show (CES) in Las Vegas, January 7-10. IDT’s wireless power transmitter and receiver IC solutions address magnetic induction- and resonance-based standards that facilitate cable-free battery charging in a myriad of portable electronic applications.
“We’re looking forward to demonstrating our industry-leading products and prototypes at CES,” said Arman Naghavi, vice president and general manager of the Analog and Power Division at IDT. “Since last year’s show, we’ve won numerous awards and announced several exciting new products. This includes the industry’s first dual-mode wireless power receiver capable of communicating with both a Qi- and PMA-type transmitter, and WPC 1.1-compatible wireless power transmitters supporting triple-coil configurations. These products, including our PMICs and other unannounced wireless power solutions will be on display for our invited customers.”
Among the products announced during 2013 is the IDTP9021, the industry’s first dual-mode wireless power receiver IC that provides compatibility with both the Power Matters Alliance (PMA) and Wireless Power Consortium (WPC) standards. IDT’s innovative receiver bridges the technology gap between competing wireless power standards, empowering OEMs to use a single bill-of-materials (BOM) for a seamless customer experience.
The IDTP9035A and IDTP9036A wireless power transmitter ICs are certified to meet the requirements of the WPC 1.1 specification for Tx-A5 and Tx-A11 (5 V single-coil), and Tx-A6 (12 V triple-coil) configurations, respectively. On the receive side, the IDTP9025 is a single-chip WPC-certified IC, including an onboard synchronous full-bridge rectifier and low-resistance low-dropout (LDO) regulator, enabling customers to achieve excellent power transfer efficiency with minimal external component count and board space.
Other pre-announced products and magnetic resonance-based wireless power information will be accessible to invited guests only. Please contact your local IDT sales representative for more information. To learn more about IDT’s announced industry-leading wireless power ICs, visit www.wirelesspowerbyidt.com.
In addition, IDT will be supporting the Alliance for Wireless Power (A4WP) and its Rezence brand launch in the A4WP meeting room located at S213. IDT will also be supporting the WPC in booth SL-2 and the PMA in booth 30242. All booths are located in the South Hall of the Las Vegas Convention Center.
About IDT Wireless Power
IDT is a leader in wireless power transmitter and receiver solutions for wireless charger applications, addressing all major standards and technologies with an extensive portfolio of standards-certified products. IDT has proven expertise in both magnetic induction and magnetic resonance technologies, and actively participates in the Wireless Power Consortium (WPC), Power Matters Alliance (PMA), and Alliance for Wireless Power (A4WP) as a board member. IDT has introduced a number of innovative and award-winning products, including the first true single-chip transmitter, the highest-output-power single chip receiver, and the first dual-mode receiver IC compatible with both WPC and PMA standards. Prominent industry players have recognized this leadership and partnered with IDT as their silicon vendor for next-generation wireless power solutions.
About IDT
Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.
###
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.