IDT’s New Family of Integrated Mixed-Signal, Low-Power Devices Reduces Bill of Materials and Application Footprint in Mobile and Embedded Systems

2012年3月10日

SAN JOSE, Calif., October 12, 2011 – Integrated Device Technology, Inc. (IDT®; NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that it has released the industry’s first integrated timing, thermal sensor and fan control solution targeted at PC mobile platforms, digital video recorders (DVRs), set top boxes (STBs), Network Attached Storage (NAS) and enterprise Ethernet switches and routers. The new family of devices reduces bill of materials (BOM) and application footprint to save cost and free-up valuable board space in densely populated enclosures.

       The IDT 9TCS108x devices integrate a low-power system timing solution, two-channel thermal sensor, and four-wire pulse width modulation (PWM) fan controller on a single chip. The low-power PLL design extends battery life in portable applications, while the multiple clock outputs of the device can replace on-board crystals to reduce physical size and weight.

          “IDT’s new integrated timing and thermal management solution takes a system-level approach to bring value to the application,” said Ram Iyer, vice president and general manager of the Computing and Multimedia Division. “We’ve leveraged our timing expertise and combined it with precision analog functions to simplify our customers’ designs, resulting in a space-saving, lower-cost solution that allows our customers to get to market sooner.”
 
          The integrated thermal sensor features two channels with ±1°C accuracy to detect overheating conditions and improve system reliability. A separate temperature alert function for each channel can be programmed to generate reference data for the fan controller or an alert signal for the system, providing design flexibility for different applications.

          In addition, the fan controller allows for direct fan control without requiring a system interrupt or supplementary control circuitry, further simplifying the design. The new family of devices offers a number of output and frequency variants, including common frequencies of 24MHz, 25MHz, 27MHz, 48MHz and 32.768KHz which consumes less than 2uA of supply current during battery powered mode. The options also provide additional thermal sensors and other control pins, allowing system designers to choose the device best suited to their application.

Pricing and Availability
          The IDT 9TCS1082, 9TCS1083, and 9TCS1085 are currently sampling to qualified customers and are available in a 5x5mm 32-ld QFN package. The IDT 9TCS108x family pricing starts at $2.50 each for volumes of 10,000 units, with different prices for different options. For more information, please visit www.idt.com/go/MobileAccess.

About IDT
          Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com . Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.