New Solution Achieves Total Frequency Accuracy of 100ppm and Below

2013年9月9日
SAN JOSE, Calif., October 21, 2010 – Integrated Device Technology, Inc. (IDT®; NASDAQ: IDTI), the Analog and Digital Company delivering essential mixed-signal semiconductor solutions, today announced the industry’s most accurate all-silicon CMOS oscillator, which achieves an industry-leading 100ppm total frequency error across temperature, voltage and other factors.
Using the patented IDT CMOS oscillator technology, the IDT3C02 oscillator replaces quartz crystal-based oscillators with a monolithic CMOS IC at a frequency accuracy of 100ppm and below, and at very thin form factors without the use of any mechanical frequency source or PLL. The product is specifically designed to work with next-generation storage, datacom and connectivity interfaces, such as 1Gb Ethernet, SAS, SuperSpeed USB (USB 3.0) and PCI Express. The product is a low-power, low-jitter replacement to general-purpose quartz crystal oscillators, making it ideal for server and enterprise designs as well as datacom devices with Ethernet ports.
“With its sub-100ppm total frequency error, the IDT3C02 is a major breakthrough in the timing industry” said Fred Zust, vice president and general manager of the Communications division at IDT. “An ideal choice over crystal alternatives, it expands on the all-silicon CMOS oscillators in wafer forms announced earlier this year and extends the IDT timing leadership.”
The IDT3C02 oscillator generates highly accurate frequencies on chip without relying on a piezo-electric or mechanical resonator. Built on a standard, readily available CMOS process, the device utilizes a programmable architecture and supports various configuration options to suit a broad range of applications. Perhaps most critical among these options is the frequency of operation, which is programmed by the factory and allows for shorter lead times, including unique or uncommon frequencies, compared with traditional quartz solutions.
In addition, the IDT3C02 oscillator is designed with a unique analog core, which consumes less than 2.5mA (unloaded, typical), and thus offers a lower power alternative to high frequency quartz- and PLL-based oscillators while delivering best-in-class -140dBc/Hz phase noise at 1MHz offset from carrier. The device is offered in industry-standard quartz crystal-compatible package of 5x3.2mm, but eliminates the need for hermetically sealed ceramic packaging and instead utilizes low-cost and thin-profile MSL1 plastic IC packaging.
The IDT3C02 also features a 200nA (typical) low power stand-by mode, and fast start-up time of 100us (typical). The combination of these features makes it ideal for power-sensitive designs and allows for frequent power cycling for further power savings. Because the device contains no moving elements and generates the frequencies electronically instead of using mechanical or piezo-electronic resonance, the all-silicon, monolithic implementation leads to excellent shock and vibration resistance.
Pricing and Availability
The IDT3C02 is currently sampling to qualified customers and is available in a 5x3.2mm package. The IDT3C02 is priced at $0.73 each in 1,000-unit quantities. For more information, please visit www.idt.com/go/CMOS-Oscillators.
Integrated Device Technology, Inc., the Analog and Digital Company™, combines analog and digital technology to develop system-level innovations that optimize customers’ applications and enrich the end-user experience. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Twitter and Facebook.
 
###
 
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.