IDT’s CrystalFree High-performance Piezoelectric MEMS Clock Generators Offer a Consolidated, Low-power, Two-output Solution for Industrial, Cloud Computing and Mobile Applications
一月 30, 2012

SAN JOSE, Calif., January 30, 2012 – Integrated Device Technology, Inc. (IDT®; NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced the world’s first low-power, multi-output PLL clock generators using IDT’s patented Piezoelectric MEMS (pMEMS™) technology. The new devices expand IDT’s leading timing portfolio by consolidating the function of two crystal oscillators, completely eliminating the need for external crystals and oscillators. This enables customers to significantly simplify their designs and reduce the bill-of-materials (BOM) in a myriad of general purpose applications, including industrial, cloud computing and mobile. 

          The IDT5V8001x and IDT5V8002x families are high-performance single- and dual-output ±50 ppm timing devices incorporating IDT’s CrystalFree™ pMEMS resonators. Combined with IDT’s ultra-low-power PLL technology, this family of devices provides two independent single-ended output frequencies at up to 200 MHz, allowing system designers to reduce component count, save board space, simplify trace routing, and lower testing costs. The multi-output devices consume up to 75 percent less power than competitive two-output spread spectrum-enabled MEMS timing solutions, making them well-suited for battery-powered portable devices or cooling-hungry enterprise datacenters. These pMEMS-based clock generators offer superb reliability in standard 3x3 mm QFN packaging and operate across the full industrial temperature range.

          “Our new CrystalFree pMEMS-based clock generators redefine the standard for high-performance, easy-to-use timing solutions and grow IDT’s portfolio of products and technologies that address the $4B frequency control market,” said Fred Zust, vice president and general manager of the Timing and Synchronization Division at IDT. “By eliminating the crystal and integrating the PLLs, we’ve taken the ambiguity out of building a timing solution, and consolidated the outputs into a single device with a smaller footprint. Our growing pMEMS portfolio further strengthens our leadership position in timing and delivers the highest level of innovation to advance our customers’ next-generation designs.”
 
          Some of the new clock generator devices feature spread spectrum capability that can be toggled using hardware select pins, allowing the designer to reduce electro-magnetic interference (EMI) in-system during compliance testing, rather than redesigning the whole board. In addition, the devices operate with only 75 ps of short-term cycle-cycle jitter, meeting the demands of high-performance PC and consumer markets.

Pricing and Availability
          The IDT IDT5V8001x and IDT5V8002x families are currently sampling to select customers. For more information about IDT pMEMS, visit www.idt.com/go/pMEMS.

About IDT
        Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on FacebookLinkedInTwitter, and YouTube.


###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.