IDT Expands NVM Express Controller Portfolio with NVMe Non-volatile DRAM Solution, Maximizing Random Performance While Reducing Latency in Enterprise Applications

2012年9月6日

SAN JOSE, Calif., September 6, 2012 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced the industry’s first NVM Express (NVMe) enterprise non-volatile DRAM (NV-DRAM) controller with native support for PCIe® Gen 3. The new NVMe NV-DRAM controller expands upon IDT’s previously announced NVMe flash controller family to provide standards-based, high-density, high-performance PCIe-attached NV-DRAM solutions built around a combination of DRAM and NAND flash devices.

          The IDT 89HF08P08AG3 NV-DRAM controller supports up to 32 GB of DDR3 SDRAM and 8 channels of NAND flash, with a PCIe x8 Gen 3 host interface. The controller is designed to fully comply with the NVMe standard – a standard that defines an optimized register interface, command set, and feature set for PCIe-based solid-state drives (SSDs). IDT’s new PCIe NV-DRAM controller enables unparalleled read and write random performance with extremely low latency and high endurance, making it ideal for storage-intensive enterprise-class applications. The programmable controller provides OEMs the flexibility to quickly develop and deploy NV-DRAM solutions that use standard NVM Express drivers.

          “IDT continues to be at the forefront of NVMe PCI Express controller innovation. The new NVM Express NV-DRAM controller follows the industry’s first NVMe enterprise flash controller announced in August,” said Kam Eshghi, senior director of marketing of the Enterprise Computing Division of IDT. “IDT’s family of NVMe flash and NV-DRAM controllers dramatically boosts the number of random I/O operations per second (IOPS) that a system can process. At the same time, the devices eliminate the traditional SAS and SATA storage infrastructure and thereby reduce latency, power and cost. NVMe is enabling a paradigm shift occurring in enterprise architectures and IDT’s NVM Express controllers play a central role.”

          The 89HF08P08AG3 NV-DRAM controller reads and writes data directly into DDR3 DRAM at speeds of up to 3 GBps. When the 89HF08P08AG3 controller detects power-down, the DRAM contents are backed up into NAND flash. With up to eight NAND flash channels and eight targets per channel, this backup operation can be performed with a write bandwidth of up to 1 GBps, depending on flash type and number of targets utilized. The 89HF08P08AG3 supports up to 32GB of DDR3 SDRAM, with configurable data rate from DDR3-800 through DDR3-1600. The datapath is 72 bits wide (64 b data and 8 b ECC) with four ranks, and it supports x8 and x16 SDRAM data widths.

          As with IDT’s PCIe flash controllers, the new PCIe NV-DRAM controller is fully programmable, enabling customers to differentiate their solutions with custom firmware that leverages IDT’s reference firmware. In addition, IDT’s 89HF08P08AG3 provides the data integrity and reliability features expected in enterprise-class solutions.

          IDT’s NVMe flash controllers will be on display at the Intel Developer Forum, September 11-13, in San Francisco, California. For more information about the NVMe specification, visit www.nvmexpress.org.

Availability
          The IDT 89HF08P08AG3 is currently sampling to qualified customers and is available in a 25 x 25 mm FCBGA. For more information about IDT’s world-class portfolio of PCIe switches, bridges, clocks, signal integrity products, and flash and NV-DRAM controllers, visit www.idt.com/go/PCIe.

About IDT
         Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.