IDT’s Patent-protected Compression IP Reduces System Cost by Enabling the Use of Low Cost Fiber to Connect RRUs to Baseband Unit in Wireless Infrastructure
2013年2月26日
SAN JOSE, Calif., February 21, 2012 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced data compression intellectual property (IP) that offers the industry’s highest performance in 3G and 4G wireless infrastructure applications. IDT’s patent-protected baseband data compression IP reduces system cost by enabling the use of low cost fiber optic cabling to connect the remote radio unit (RRU) to the baseband unit (BBU).
In an industry where performance and cost demands pull strongly in opposite directions, wireless communication equipment manufacturers are looking for solutions to pass increasing amounts of data over inexpensive, low-speed fiber optic cable links (up to 2.5 Gbps). IDT’s data compression IP solves this dilemma by offering compression ratios from 2:1 to 4:1, enabling customers to utilize low-cost cabling by reliably compressing data while keeping overall signal quality within required wireless parameters. IDT’s compression IP is the only IP in the industry achieving 3:1 compression at the error vector magnitude (EVM) percentage required in 4G systems at full Common Public Radio Interface (CPRI) line rates. The data compression IP is available as an FPGA or ASIC instantiation suitable to support GSM, WCDMA, and LTE systems.
“Our industry-leading compression IP offers our customers the tools and support they need to develop high-performance and cost-effective wireless communication solutions,” said Tom Sparkman, vice president and general manager of the Communications Division at IDT. “With 4G-compliant EVM rates at a 3:1 compression ratio, the value proposition of IDT’s compression IP is highly attractive to all BBU manufacturers looking for a competitive advantage. Coupled with our Serial RapidIO interconnect, RF signal path, timing, and high speed data converter products, IDT offers the industry’s most complete and compelling wireless signal chain solutions on the market.”
IDT’s compression IP operates with sub-microsecond latency for the entire compression and decompression chain, having negligible impact on overall system performance. Furthermore, while the compression IP is typically used to compress data on the link between the RRU and BBU in radio access networks, it can also be used to compress data in repeater systems on the link between master and slave units. This provides customers the opportunity to use fewer fiber links and optical connectors to save considerable cost and power.
Pricing and Availability
The IDT’s data compression IP is currently sampling to qualified customers as an FPGA demonstration kit. For more information about IDT’s compression IP, visit www.idt.com/go/CompressionIP.
About IDT
Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.
“Our industry-leading compression IP offers our customers the tools and support they need to develop high-performance and cost-effective wireless communication solutions,” said Tom Sparkman, vice president and general manager of the Communications Division at IDT. “With 4G-compliant EVM rates at a 3:1 compression ratio, the value proposition of IDT’s compression IP is highly attractive to all BBU manufacturers looking for a competitive advantage. Coupled with our Serial RapidIO interconnect, RF signal path, timing, and high speed data converter products, IDT offers the industry’s most complete and compelling wireless signal chain solutions on the market.”
IDT’s compression IP operates with sub-microsecond latency for the entire compression and decompression chain, having negligible impact on overall system performance. Furthermore, while the compression IP is typically used to compress data on the link between the RRU and BBU in radio access networks, it can also be used to compress data in repeater systems on the link between master and slave units. This provides customers the opportunity to use fewer fiber links and optical connectors to save considerable cost and power.
Pricing and Availability
The IDT’s data compression IP is currently sampling to qualified customers as an FPGA demonstration kit. For more information about IDT’s compression IP, visit www.idt.com/go/CompressionIP.
About IDT
Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.
###
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.