ZL8801 Dual Phase Digital PWM Controller Demo

Added on 2015-03-28

The ZL8801 dual-phase, DC/DC digital PWM controller leverages the patented ChargeMode control loop architecture to deliver transient response performance that's far superior to today's analog controllers.


関連ビデオ

6:06
This video provides an introduction to the ZL8801 dual phase digital DC/DC controller.
4:00
This video explains the connections required for the ZL8801 dual phase digital DC/DC controller’s current sharing applications.
1:24
Learn how to use the ISL99140 DrMOS FET driver with the ZL8801 digital power controller.
4:38
This video provides a demonstration of the ZL8801 4-phase digital DC/DC controller demo board.
1:40
In this video, the differences between the ZL8800 and ZL8801 dual phase PMBus™ ChargeMode™ control DC/DC digital controllers are identified.
1:28
This video introduces the ZL8801 dual phase DC/DC digital PWM controller.
6:06
This video provides an introduction to the ZL8801 dual phase digital DC/DC controller.
4:00
This video explains the connections required for the ZL8801 dual phase digital DC/DC controller’s current sharing applications.
1:24
Learn how to use the ISL99140 DrMOS FET driver with the ZL8801 digital power controller.
4:38
This video provides a demonstration of the ZL8801 4-phase digital DC/DC controller demo board.
1:40
In this video, the differences between the ZL8800 and ZL8801 dual phase PMBus™ ChargeMode™ control DC/DC digital controllers are identified.
1:28
This video introduces the ZL8801 dual phase DC/DC digital PWM controller.
6:06
This video provides an introduction to the ZL8801 dual phase digital DC/DC controller.
4:00
This video explains the connections required for the ZL8801 dual phase digital DC/DC controller’s current sharing applications.
1:24
Learn how to use the ISL99140 DrMOS FET driver with the ZL8801 digital power controller.
4:38
This video provides a demonstration of the ZL8801 4-phase digital DC/DC controller demo board.
1:40
In this video, the differences between the ZL8800 and ZL8801 dual phase PMBus™ ChargeMode™ control DC/DC digital controllers are identified.
1:28
This video introduces the ZL8801 dual phase DC/DC digital PWM controller.

ビデオのトランススクリプト

Hello, my name is Philip McKenzie. I'm here at APEC 2015 demonstrating the ZL8801 two-phase fully digital controller.

On the screen behind me, I have a running version of our PowerNavigator GUI that we use to help configure the device and show its general features and capabilities. The board I'm using to demonstrate is a four-phase version of our ZL8801. The ZL8801 can be used in two-phase, four-phase, six-phase, and eight-phase configurations. And in addition, we have a two-phase version that's also available. The two-phase version has a smart power device, the ISL99140. It's a 6mm x 6mm DrMOS type device capable of 40A per channel.

Using the PowerNavigator interface, you have the ability to configure the device for operations such as sequencing. Also, have the ability to change the turn-on and turn-off times by simply moving the cursor over the grab point and changing the on and off times or even the delay times.