Added on 2014-09-26

How to use the ISL99140 DrMOS FET driver with the ZL8801 digital power controller.


関連ビデオ

6:06
This video provides an introduction to the ZL8801 dual phase digital DC/DC controller.
4:00
This video explains the connections required for the ZL8801 dual phase digital DC/DC controller’s current sharing applications.
1:24
Learn how to use the ISL99140 DrMOS FET driver with the ZL8801 digital power controller.
4:38
This video provides a demonstration of the ZL8801 4-phase digital DC/DC controller demo board.
1:40
In this video, the differences between the ZL8800 and ZL8801 dual phase PMBus™ ChargeMode™ control DC/DC digital controllers are identified.
1:28
This video introduces the ZL8801 dual phase DC/DC digital PWM controller.
6:06
This video provides an introduction to the ZL8801 dual phase digital DC/DC controller.
4:00
This video explains the connections required for the ZL8801 dual phase digital DC/DC controller’s current sharing applications.
1:24
Learn how to use the ISL99140 DrMOS FET driver with the ZL8801 digital power controller.
4:38
This video provides a demonstration of the ZL8801 4-phase digital DC/DC controller demo board.
1:40
In this video, the differences between the ZL8800 and ZL8801 dual phase PMBus™ ChargeMode™ control DC/DC digital controllers are identified.
1:28
This video introduces the ZL8801 dual phase DC/DC digital PWM controller.
6:06
This video provides an introduction to the ZL8801 dual phase digital DC/DC controller.
4:00
This video explains the connections required for the ZL8801 dual phase digital DC/DC controller’s current sharing applications.
1:24
Learn how to use the ISL99140 DrMOS FET driver with the ZL8801 digital power controller.
4:38
This video provides a demonstration of the ZL8801 4-phase digital DC/DC controller demo board.
1:40
In this video, the differences between the ZL8800 and ZL8801 dual phase PMBus™ ChargeMode™ control DC/DC digital controllers are identified.
1:28
This video introduces the ZL8801 dual phase DC/DC digital PWM controller.

ビデオのトランススクリプト

Hello, my name is Brandon Howell, and I handle technical marketing with Renesas' Digital Power Group. Today, we're gonna be talking about the benefits of using ISL99140 DrMOS power stage with ZL8801 digital power controller.

You noticed that the ZL8801 controller has PWM outputs for driving an external power stage. In this case, we're driving the ISL99140 DrMOS power stage. DrMOS means the power stage has both the driver and MOSFETs integrated in one package.

There are some benefits to doing it this way. By having a driver in the same package as the MOSFETs, you reduce the overall parasitics. This allows for higher efficiency and lower noise coming from the power stage. It also simplifies your layout. Because we only provide PWM signal to the driver, we have no high current path from the controller to a DrMOS power stage. This really simplifies the layout and allows extra flexibility in placing the power stage.