このプロジェクトは、UARTインターフェースを介して接続された外部サイレックスULPGN Wi-Fiモジュールを使用することで、Wi-Fi接続機能の追加を可能にします。

詳細

このプロジェクトでは、サイレックスSX-ULPGN-EVK Wi-Fi評価キットに接続したRenesas Synergy™ プラットフォームのデモンストレーション例を提供します。デモンストレーションにはSX-ULPGN Wi-Fiフレームワーク・アプリケーション・プログラミング・インターフェース(API)も含まれています。また、オンチップのソフトウェア・スタックとAPI、SK-S7G2開発ボード用ソケットAPIも含みます。SX-ULPGNは チップ搭載型Qualcomm QCA4010 (SoC)をベースとした2.4 GHz 802.11n対応モジュールのシングルボードです。

SX-ULPGN

Copyright Disclaimer

Copyright © 2018 Silex. All Rights Reserved.

The content included herein has been provided by other companies and Renesas does not claim any ownership therein. Renesas may or may not moderate or pre-screen the content included herein. Renesas requires partners to verify the functionality of their products on Synergy Platform and Renesas is not responsible in any way for the content included herein nor its quality. Renesas does not endorse any content included herein or any opinion, recommendation, or advice expressed therein, and Renesas expressly disclaims any and all liability in connection with such content, whether or not arising under the laws of copyright, libel, privacy, obscenity, or otherwise. Renesas does not provide support for any of this content; all support requirements should be directed to the owner or licensor of the content. Renesas retains the right, at its sole discretion and without prior notice, to pre-screen, refuse, or remove any content from the Synergy Platform.

/ja/products/synergy/gallery/partner-projects/silex-wifi-pmod/jcr:content/gallerydownload

バージョン 1.0

現在のリリース

リリース日: 2018-03-08

対応MCU: S7G2, S3A7, S3A3, S5D9, S5D5, S5D3, S3A6, S3A1

MD5: 0e1bc009c3ddb4b65ee68ed717c7af67

ダウンロード

インストール手順

  • wifi-addon-installer.exe – Installation executable to install the CMSIS pack file for the ULPGN drivers for Renesas Synergy
  • ulpgn_demo-20171218.zip – project file archivetcpserver.c – Additional optional file for use with the demo project, to set up a demonstration TCP server
  • udpserver.c – A UDP version of tcpserver.c

Detailed instructions are provided in the quick start guide with application note, driver code and demo is included.

ドキュメンテーションとサポート

/ja/products/synergy/gallery/partner-projects/silex-wifi-pmod
/ja/products/synergy/gallery/partner-projects/silex-wifi-pmod/jcr:content/allversionsection