IDT’s System-on-Chip (SoC) Boasts Industry’s Widest Dynamic Range with Integrated Energy Metering Analog Front End, Real-time Clock, Temperature Sensor, LCD Driver and Microprocessor
SAN JOSE, Calif., March 20, 2012 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced the world’s most advanced single-phase power metering SoC for smart grid applications. This new device features the industry’s widest dynamic range and an unprecedented level of integration, enabling smart meter manufacturers to improve accuracy, while simplifying their designs and lowering overall system cost.
The IDT 90E46 is a single-phase SoC for smart meter designs, which integrates an energy metering analog front-end with a real-time clock, temperature sensor, LCD driver, and ARM Cortex M0 microprocessor. The metering device is the latest member of IDT’s award-winning family and offers the industry’s widest dynamic range of 5000:1, which enables meter manufacturers to merge various meter types into one, thus simplifying the design and manufacturing process for meter makers and reducing the storage and management complexity for utilities. The high level of integration enables system designers to significantly simplify the hardware design and lower the bill-of-materials (BOM) cost.
“IDT is the only company to offer such a high-performance and highly integrated device for the smart meter market,” said Sean Fan, vice president and general manager at IDT. “Our original energy metering products have proven very successful with customers and have garnered multiple awards. With our expertise in analog and digital technology, we anticipate continued success with this unparalleled next-generation product for the booming smart grid market.”
The new IDT metering SoC is fully compliant with international (both IEC and ANSI) and Chinese standards, and meets or exceeds the requirements set forth by the State Power Grid Corporation of China (SGCC). The device features 128 kB of internal flash memory, enabling users to store large instruction sets for the integrated microprocessor.
Pricing and Availability
The IDT 90E46 is currently sampling to qualified customers, and is available in a 100-pin TQFP package. The IDT 90E46 is priced at $2.50 each for volumes of 10,000 units. For more information about IDT’s power metering portfolio, visit www.idt.com/go/PowerMeter.
About IDT
Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.
###
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.