Sponsored by IDT, Registration is Now Open for the Unique New Sport that Splits a 15K Race into 2 Legs

2015年1月20日

SAN JOSE, Calif., Jan. 20, 2015 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) announced today that registration is open for the Double Racing Festival’s return to San Jose. The centerpiece of the unique family-friendly festival on Feb. 21 is the Double Road Race 15K, which splits the race into two legs—a 10K and a 5K, with a break in between. It’s “the only running event with a halftime,” says creator Bob Anderson, founder of Runner’s World magazine.

IDT is again the primary sponsor of the San Jose event, which will feature live music and food. Double racing is run at various locations in the United States throughout the year, and has been held at international locations as well, including Greece and Kenya.

The San Jose race begins and ends at IDT headquarters in south San Jose.  Times from the two legs are combined for scoring.  All Double Road Race finishers receive a medal, high-performance shirt, and a draw-string tote bag.

Two other racing events are scheduled alongside the Double Road Race 15k. The UjENA Double 5K features a 3K leg and a 2K leg. Children 13 and younger can participate in the 1.5-mile Kids Cup Double, with a 1-mile leg followed by a half-mile leg. All races include a halftime.

“The Double Racing Festival is a great event for runners—and walkers--at all levels and ages,” said Leslie Garcia of IDT. “IDT encourages and facilitates healthy living for our employees, and sponsoring this event is a perfect fit for a company that’s been selected a Bay Area Healthy Employer for four years running.”

For more information about the race and to register, visit www.SanJoseDouble.com.  IDT headquarters is located at 6024 Silver Creek Valley Road.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

この記事をシェアする