This embedded configuration demo makes full use of the functionality of the RL78/G1D microcontroller. One RL78/G1D microcontroller can easily be used to build an embedded system for running applications and Bluetooth operations. This video shows two RL78/G1D evaluation boards. They mutually control each other’s LEDs with one board acting as the central board and the other as the peripheral.