Integrated Automotive Cockpits

Renesas Automotive TechDays 2019

Save cost and design effort in functional safety with Renesas scalable R-Car roadmap, providing a robust freedom of interference between the Cluster and Android system.

Related Videos

1:57
Take a glimpse of the Automotive TechDays 2019. A great chance for customers to interact with Renesas product experts and discover available Digital and Analog solutions.
2:26
Discover Vehicle Computer 2, the complete evaluation platform, that enables quick prototyping with Renesas’ Digital and Analog chipsets and CETITIC software stack.
1:33
Find out how Renesas’ MCU high speed flash architecture enables over-the-air software updates while the actual code is running. Save time during software maintenance.
2:08
Charging mobile devices in vehicles can be much safer and more convenient with the Renesas wireless power transmitter designed for automotive applications.
1:39
Save cost and design effort in functional safety with Renesas scalable R-Car roadmap, providing a robust freedom of interference between the Cluster and Android system.
1:34
Reduce development time by more than six months with the use of the reference design containing both Battery Management IC (ISL78714) and ASIL-D rated MCU (RH850/P1M).
1:52
See how Renesas’ clock solutions can help meet system requirements and provide ease of use for configuration.
1:38
Renesas’ sensor signal conditioners (SSCs) are cost efficient and flexible solutions for automotive designs.
1:57
Take a glimpse of the Automotive TechDays 2019. A great chance for customers to interact with Renesas product experts and discover available Digital and Analog solutions.
2:26
Discover Vehicle Computer 2, the complete evaluation platform, that enables quick prototyping with Renesas’ Digital and Analog chipsets and CETITIC software stack.
1:33
Find out how Renesas’ MCU high speed flash architecture enables over-the-air software updates while the actual code is running. Save time during software maintenance.
2:08
Charging mobile devices in vehicles can be much safer and more convenient with the Renesas wireless power transmitter designed for automotive applications.
1:39
Save cost and design effort in functional safety with Renesas scalable R-Car roadmap, providing a robust freedom of interference between the Cluster and Android system.
1:34
Reduce development time by more than six months with the use of the reference design containing both Battery Management IC (ISL78714) and ASIL-D rated MCU (RH850/P1M).
1:52
See how Renesas’ clock solutions can help meet system requirements and provide ease of use for configuration.
1:38
Renesas’ sensor signal conditioners (SSCs) are cost efficient and flexible solutions for automotive designs.
1:57
Take a glimpse of the Automotive TechDays 2019. A great chance for customers to interact with Renesas product experts and discover available Digital and Analog solutions.
2:26
Discover Vehicle Computer 2, the complete evaluation platform, that enables quick prototyping with Renesas’ Digital and Analog chipsets and CETITIC software stack.
1:33
Find out how Renesas’ MCU high speed flash architecture enables over-the-air software updates while the actual code is running. Save time during software maintenance.
2:08
Charging mobile devices in vehicles can be much safer and more convenient with the Renesas wireless power transmitter designed for automotive applications.
1:39
Save cost and design effort in functional safety with Renesas scalable R-Car roadmap, providing a robust freedom of interference between the Cluster and Android system.
1:34
Reduce development time by more than six months with the use of the reference design containing both Battery Management IC (ISL78714) and ASIL-D rated MCU (RH850/P1M).
1:52
See how Renesas’ clock solutions can help meet system requirements and provide ease of use for configuration.
1:38
Renesas’ sensor signal conditioners (SSCs) are cost efficient and flexible solutions for automotive designs.


Video Transcript

My name is Guido Hilker, I'm from Renesas Electronics and today I talk about integrated cockpits.

The challenge of integrated cockpit is to run cluster, navigation and center stack on one ECU. Some OEMs have already started such integration with the target to save cost and still offer an attractive solution with a nice look and feel.

The demo is running on R-Car M3N and is showing a low cost integrated cockpit solution. In the middle, an Android system is running, showing a navigation application which could be also a smartphone replication. In parallel, the embedded real-time CPU, which is separated by system architecture, is drawing a full graphics cluster using the 2D drawing engine.

For integrated cockpit, Renesas offers a scalable R-Car product lineup. And also robust freedom of interference between the cluster system and the Android system is achieved by separation of hardware. And therefore the efforts for functional safety can be greatly reduced, which saves cost and effort. Finally, the real-time system will boot faster, offering an early availability of the cluster function, rearview camera or audio.