Statement on REACH Regulation

Compliance

Renesas is aware of the REACH regulation and will take all necessary actions to fully comply with its requirements, especially Title VIII § 67 and Annex XVII.

Pre-Registration / Registration

  1. Renesas semiconductor devices do not exhibit intended release of chemical substances (listed in Annex XVII*) under normal or reasonably foreseeable conditions of their application. In line with the REACH regulation there will be NO need to register any substance.
  2. Following the in-depth evaluation of the chemical substance content in our products Renesas confirms that Renesas devices except products mentioned on the following PDF do not contain any SVHC-candidates.

Impact on Availability of Products

Renesas confirms to undertake all necessary efforts to comply with REACH regulation to ensure continuous supply of Renesas products to our valued customers.

Updates

The REACH cert is to be updated whenever new SVHC are added; it will take two months from the date when the new SVHC are added.

Documentation & Downloads