Download (D4000360)

Issue Date : Jan.20.17

Category : Evaluation Software, Compiler Upgrades

RX Family C/C++ Compiler Package V2 (without IDE) V2.06.00

Description

For the description of the RX Family C/C++ Compiler Package V2 (without IDE), see Product Information.

This product is the commercial edition of the C/C++ Compiler Package for RX Family (IDE and a simulator are not included).

Use this as an updater of the compiler without IDE.

Click below for detailed information.

 

How to Install

This updater can be applied to CS+ for CC common program V4.00.00 or later.

The installer is invoked by executing the downloaded file. (Note: Make sure the work directory has enough space in the hard disk drive.) Follow the instruction by the installer and complete the installation. After installation, the downloaded file will no longer be used. If necessary, make a backup of the file.

 

Notes on updating your product
Install V 2.00.00 or later of License Manager.
If you don't install it, compiler will generate the warning messages and operate as the evaluation edition.
When you use a Floating License, you also need to install V 2.00.00 or later of Floating License server.

 

Notes on evaluation version

Usable as a evaluation version without registration of License Key.

 

  • Valid Period and Limitation
    The evaluation version of C/C++ Compiler Package for RX Family is provided with the same functionality as the commercial version except that link size will be restricted to 128 Kbytes on and after the 61st day from when you begin using the compiler(*). For details, please refer to Evaluation Version Software Information before downloading!!

    * Note: Even if you upgraded the old version of your compiler to the new one, the valid period is not extended.

     

  • Operational Environment

    Host machine *1 IBM PC compatible machine
    OS *2, *3 Windows® 10, Windows® 8.1, Windows® 7
    Memory capacity 128 MB at least, 256 MB or more recommended.
    Available hard disk space 150 MB or more
    Display SVGA or higher
    I/O device CD-ROM drive
    Others Mouse or compatible pointing device

    *1.IBM is registered trademarks of International Business Machines Corporation.

    *2.Windows® is registered trademarks of Microsoft Corporation in the U.S. and other countries.

    *All other company names and product names are trademarks or registered trademarks of corresponding companies.


    Additional Notes
    1. The directory or file name which comprised of ASCII character-code only can be used.
    2. A period (.), indicating an extension, can be used only once in a file name.
    3. Assign the installation path to the internal drive.
    4."Short cuts" cannot be used.
    5. No more than 1 upper directory can be specified using "...".

Download

Product Name File Name File Size Download Link
RX Family C/C++ Compiler Package V2 (without IDE) V2.06.00 CC-RX_V20600_setup.exe 21.79 MByte