Skip to content

renesas-rz/rza1_gcc_azure_rtos_bsp

Repository files navigation

RZA1 Microsoft Azure SDK

This is the RZA1 Software Development with Microsoft Azure Support. The SDK contains the RZA1 Board Support Package and drivers for the RZA1 LU, LC, L, M, and H target Processors, the Asure RTOS ( Threadx), Azure middleware ( USB Host, USB Device, Network, IoT, Filesystem, GUI Development). In driver GPIO code generation has been integrated with the RZA1 Smart Configurator.

Required Software

  • GNU ARM Compiler version 6.3.1.2017062
  • IDE Renesas e2studio

Microsoft Azure Libraries

The Microsoft Azure software is supported by the Azure Microsoft Team. This repository includes the library debug binaries. The full source code for the listed libraries can be found here.

License

  • Threadx

    This is the Microsoft Azure RTOS

  • USBx

    This is the USB middleware. It support both Host and Device. USB Class support include HID, MSC, CDC, HUB, UVC, Audio, and printer.

  • GUIx

    This the GUI middleware. It supports 16, 24 and 32 bit color space. Resolution is dependent on the amount of internal memory ( i.e. 2MB RZA1LC - 10MB RZA1H ) or external memory.

  • FileX

    This is the RTOS file system. Supports RAM disk, USB and SD ( requires request form Renesas ).

  • NetXDuo

    This middware supplies the network for IP4, Ip6, TCP, UDP, HTTP, Secure Socket Layer, Crypto libraries, and many more.

  • Azure IoT

    As part of the NetxDuo the Azure IoT Cloud connectivity is included.

Microsoft Azure Demos

  • sample_threadx

    This is a simple demo of the basic threadx RTOS APIs and memory management.

  • r_sample_threadx

    This demo is similar to the sample_threadx but uses the Renesas OS Abstraction Layer

  • sample_filex_ramdisk

    This project demonstrates the FileX API for a mass storage device located on the RZA internal RAM.

  • sample_netx_duo_iperf

    This project demonstrates the NetX API running a webpage that shows the network connectivity performance.

  • sample_netx_duo_ping

    This project demonstrates the NetX Duo API that responds to ping.

  • sample_azure_iot_embedded_sdk

    This project demonstrates the Azure IoT. A license is required to access the Microsoft Azure Cloud.

  • sample_azure_iot_sdk_ping

    This project demonstrates the Azure IoT. A license is required to access the Microsoft Azure Cloud.

  • rza1h_sample_guix_home_automation

    This project demonstrates the GUIX API. The demo simulates a home automation HMI controller. This includes lights, HVAC, Door Locks, and Outdoor Weather. The project is designed for the RZA1H RSK board. The resolution is 800 x 600 with 24bpp color depth.

Renesas RZA1 BSP Board Configuration

The rz_bsp has Renesas Evaluation board and MPU settings. The file is called "mcu_board_select.h". It can be found in the rz_bsp library in the "src/renesas/application/inc" folder. The configuration allows selection for the board ( Stream-it or RSK (Display-it kit)), MPU ( RZA1H, M,L,LU,and LC) and GUIX Driver ( 16bit, 24bit, and 32bit ). Once these changes are made, a full rebuild of the rz_bsp is required.

RZA1 Smart Configuration Code Generation

The RZA1 Smart Configurator is a separate PC application software, it is designed for hardware engineers to resolve pin conflicts for the RZA1 and RZG1 processors. The RZA1 SC does not support code generation. ( NOTE : RZA2M Smart Configurator is a different configurator that is integrated with the e2studio IDE ). This Software design kit includes scripts that generated code based on the exported pin settings.

Getting Started

Demos Getting Started Guide

About

RZA1 BSP and Driver support for the Microsoft Azure IoT. This includes Azure middleware GUIx, USBx, FileX, netX, and NetDuo source code.

Resources

Stars

Watchers

Forks

Releases

No releases published

Packages

No packages published