2022-06-24

This video demonstrates how to use e² studio to enable RL78 Logic and Event Link Controller (ELCL) function to add Slave Selection (SS) to the slave receive mode of a Serial Array Unit's (SAU) 3-wire serial I/O (CSI) and achieve 4-wire SPI (Serial Peripheral Interface) communication.

0:00:00 Introduction
0:00:14 Logic and Event Link Controller (ELCL)
0:00:54 Development Environment and Application Notes
0:01:05 Create project
0:01:51 Add components

Related videos: