C base integrated development environment which cooperated with DRP closely

Hardware design environment for the integration programmer

 

Hardware design environment for the integration programmer

Our company prepares the C base integrated development environment which is closely cooperated and integrated with DRP, for DRP firmware developing.

DRP C based Integrated Development

 

The firmware development of DRP can proceed by dividing it into 2 steps.

Image of Firmware Development of STP engine

Step 1 Algorithm development

Proceed the development in C language development environment (compiler, debugger) which the customer use usual times.

 

Step 2 Firmware development of STP engine

The DRP tool directly output the firmware of DRP, from the C language (ANSI-C conformity) description that developed by step 1.

The DRP tool display the characteristics of output firmware associated with the source code of the C language .

The designer can proceed the algorithmic optimization using this information.