S4-PMIC blog

Communication Gateway/Car Server Chipset Solution with R-Car S4 and Tailored PMIC

In this blog, we will explain how Renesas contributes with the new R-Car S4 based chipset to a smarter E/E architecture in the Automotive market.

Run a motor with encoder interface by using RA6T1 motor control RSSK

Run a Motor with Encoder Interface Using the RA6T1 Motor Control RSSK

Learn how to extract the parameters of a user’s own motor using the Renesas Motor Workbench’s tuner function with the RA6T1 MCU and how to fill the parameters into the sample program.

Completing Setup in Just 30 Minutes! Introducing the New Development Environment for Connected Cars by Renesas

Completing Setup in Just 30 Minutes! Introducing the New Development Environment for Connected Cars by Renesas

Using the Connected Car Platform - Starter Kit (CCPF-SK), R-Car users can set up the development environment for connected cars easily and quickly and focus on the development of added value software.

Radar Transceivers: A Key Component for ADAS & Autonomous Driving 2 - Basics of FMCW Radar Blog

Basics of FMCW Radar

In the second entry of this series on automotive radar, the basics of automotive radar will be presented: the principle of FMCW radar, radar processing and the architecture of a radar module.

Improve UX/UI with RX140 MCU Equipped with A New Generation of Capacitive Touch Sensor

Improve UX/UI with RX140 MCU Equipped with A New Generation of Capacitive Touch Sensor

The RX140 in the RX100 MCUs contribute to improved device performance and lower power consumption and feature the latest touch-key IP to further enhance the design and usability of customer products.

Embedded Artificial Intelligence Inference with Renesas RZ/G2

Embedded Artificial Intelligence Inference with Renesas RZ/G2

Introducing the RZ/G Free and Open Source Software (FOSS) AI Board Support Package (BSP) that includes popular Open Source AI frameworks and sample benchmarking applications for each framework.

Interview with RX Family User, HITACHI Solutions Technology

Interview with RX MCU Family User, HITACHI Solutions Technology

This interview with HITACHI Solutions Technology details their adoption of the RX72N MCU for easy improvement of system performance and functionality and easy development for the long-term.

Thermopile CO₂ Detector Blog

Building an Accurate Ambient CO₂ Detector with Connectivity

The Thermopile CO₂ Detector Winning Combination is a reference design using Renesas’ RTD120D dual thermopile to detect the ambient CO₂ concentration.

Renesas Functional Safety Support for Automotive (3) – Applying the ISO 26262 Standard to SEooC Software

Renesas Functional Safety Support for Automotive (3) – Applying the ISO 26262 Standard to SEooC Software

This blog presents ISO 26262 guidance on developing Safety Element out of Context (SEooC) software, the challenges encountered during SEooC software development, and Renesas SEooC software solutions.

The RA MCU family is made to help solve your design challenges

The RA MCU Family is Made to Help Solve Your Design Challenges

The entry-level RA4E1 and RA6E1 MCUs address key design challenges including the optimal balance between performance and power consumption, as well as seamless migration options for future designs.