Renesas building security systems realize convenience and peace of mind through sensing, connectivity, and user interface technologies. In the context of building automation, security systems are composed of two constituent elements. The figure below is a conceptual diagram. The first is a monitoring system that oversees what is going on in and around the building by means of cameras and sensors of various types. The second is a crime prevention systems that perform ingress and egress management and control based on the information from the monitoring systems.

Image
Building Security Systems Illustration
Building Security Systems

Monitoring Systems

Monitoring systems may include motion sensors for ingress monitoring and fire detectors, carbon monoxide detectors, and the like to monitor for emergencies within the building. The monitored information is sent via the network to a supervisor in the form of emergency signals and images. This information can also be stored and managed on a secure data server if needed.

Crime Prevention Systems

Crime prevention systems may incorporate sensors such as door open-close detectors and glass break detectors to detect emergencies as well as ingress and egress management functions to enforce entrance and exit regulations and keep logs of those entering and leaving. They control the entrance and exit of persons to and from the building in conjunction with the information from the monitoring systems.

Communication Networks of Security Systems

Via the network, the large volumes of data making up the security logs, operation logs, and entrance and exit logs from the monitoring and crime prevention systems are tracked on security monitoring PCs and stored and managed on secure data servers. This information may also be linked via a network to other building automation systems (air conditioning systems, lighting systems, etc.) to enable more efficient building security management.

Image
Building Security Network Illustration
Building Security Network