SAN JOSE, Calif., October 25, 2011 – Integrated Device Technology, Inc. (IDT®; NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that Samsung has selected its low-power dual-port memory for use in the popular GALAXY Tab. 10.1 LTE tablet PC. IDT’s device was chosen for its ultra-low power consumption to maximize battery life.
The IDT 70P255 is a low power 8K x 16 Dual-Port Static RAM (DPSRAM). The device provides two independent ports with asynchronous access for simultaneous reads or writes to any location in memory, enabling the tablet’s baseband processor (BP) and application processor (AP) to work in concert. An automatic power down feature permits the device to enter a low-power standby mode (3.6 uW typical) to save power and extend battery life when the memory is not being accessed. Fabricated using IDT’s high-performance CMOS technology, these devices typically operate on only 27 mW of power.
“We are pleased that Samsung Electronics, a leading mobile device provider, has selected IDT’s DPSRAM for this innovative product,” said Arman Naghavi, vice president and general manager of the Analog and Power Division at IDT. “Our industry-leading low power memory products complement our highly efficient power management and world-class timing solutions. We look forward to continuing to support Samsung with our broad portfolio of mixed-signal solutions.”
The IDT 70Pxx series of devices is available in a 100-ball and 81-ball 0.5 mm pitch Ball Grid Array (BGA) with 1 mm thickness, optimized for wireless handset and portable applications. To learn more about IDT’s dual-port memory products, visit www.idt.com/go/AsyncDPRAM.
About IDT
Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.
###
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.