IDT’s Groundbreaking Wireless Power Transmitter Offering Significant Reduction in Footprint and BOM Cost Along with Innovative Receiver Is Recognized by Leading Japanese Publication

June 7, 2012

SAN JOSE, Calif., June 7, 2012 – Integrated Device Technology, Inc. (IDT®)  (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that it received the Semiconductor of the Year Award for Excellence from Semiconductor Industry News for its innovative wireless power transmitter and receiver solutions.

          “This award is a testament to the game-changing features and capabilities of the new wireless power solutions offered by IDT,” said Arman Naghavi, vice president and general manager of the Analog and Power Division at IDT. “IDT’s fully Qi-certified wireless power transmitter is currently sampling to our customers, offering a significantly reduced application footprint and bill of materials. The wireless power receiver complements the transmitter with ‘multi-mode’ operation for improved safety and added features.”

          The Semiconductor of the Year Award was founded in 1994 to praise and recognize technologies and products that contribute to the semiconductor industry, specifically those that contribute to state-of-the-art equipment important to Japan markets. The publication chose award winners from the pool of new products and technologies released between April 2011 and March 2012. IDT’s wireless power solutions were recognized in the Semiconductor Devices category.
 
          The IDTP9030 is the world’s most highly integrated single-chip wireless power transmitter available,  integrating dozens of discrete components into a highly efficient, simplified and cost-effective solution. With the IDTP9030, customers can develop Qi-compliant proprietary or multi-mode charging stations that can be deployed virtually anywhere, including homes, offices, libraries, stores, public waiting areas, automobiles, airports and airplane seats.
 
          The IDTP9020 high-efficiency single-chip wireless power receiver complements the IDTP9030 with “multi-mode” operation. It supports dynamic switching between Qi and proprietary modes with built-in protocol detection, adding to the compelling user experience of the IDTP9030.
 
          The IDTP9030 transmitter and IDTP9020 receiver ICs are currently sampling to qualified customers. For more information about these products, visit www.idt.com/go/wirelesspower.

About IDT
          Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on FacebookLinkedInTwitter, and YouTube.
 
 
###
 
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.