SAN JOSE, Calif., June 27, 2006 — IDT™ (Integrated Device Technology, Inc.; NASDAQ: IDTI), a leading provider of vital semiconductor solutions, today announced that Chelsio Communications has chosen to incorporate IDT network search engines (NSEs) into its T210 and T204 10GbE TCP/IP offload engine (TOE) reference designs targeted at server and storage systems. The Chelsio reference designs rely heavily on the feature rich IDT NSEs to allow mutual customers’ end designs more flexibility as well as the ability to utilize more CPU cycles for data center, networking storage and high performance cluster computing (HPCC) applications. The IDT NSEs also allows the Chelsio designs to increase bandwidth, improve overall performance, optimize available power budget and reduce message latency in a cost effective manner.
The IDT NSEs easily integrate into Chelsio-based designs by hooking up to the main TCP/IP offload engine application specific integrated circuit (ASIC). By offloading the compute-intensive functions, server and storage customers can focus their resources on value-added services enabling faster time-to-market. The Chelsio board-level products process complex communications protocols at 10Gbps rates, allowing host servers and storage systems to dramatically increase both application performance and communications bandwidth. The Chelsio T210 and T204 10GbE adapter products have taken advantage of the IDT NSEs performance to achieve record setting performance for both IPv6 and IPv4 networks and in both single-stream and multi-stream categories.
“Of the many NSEs we evaluated for our TOE reference designs, IDT was the only company who offered NSEs with comprehensive customer support in conjunction with a wide portfolio enabling us to meet our power, performance and cost targets. The IDT NSEs exceeded our performance requirements and the cost compelling solution made it a perfect match for our reference design,” said Kianoosh Naghshineh, president and CEO, Chelsio Communications. “The use of the IDT NSE on the Chelsio TOE offloads a well-defined compute-intensive function that allows our customers to free up their CPU resources to concentrate on their core competencies.”
Scott Sarnikowski, vice president and general manager of the IDT IP co-processor division, said, “Leveraging the Chelsio 10 GbE TOE solution with the IDT NSE provides our customers with new levels of performance that can reduce the overall complexities and costs associated with a dynamic storage solution. Chelsio is a pioneer in delivering TOE reference designs for the server and storage markets. We are excited to be aligned with Chelsio and inclusion in the Chelsio reference design illustrates the strength of our high-performance NSE devices to serve tomorrow’s server and storage needs."
IDT Network Search Engine Solutions
IDT provides a comprehensive family of NSEs that accelerate packet processing and enable intelligent application management in next-generation networking equipment. IDT offers the industry’s highest-performance NSE operating up to 250 MHz. The IDT NSE portfolio includes a family of custom devices, as well as families of NSEs with high-performance interfaces for ASICs, and glue-less interfaces to leading network processors, to accelerate packet classification and forwarding in core, metro and access networks. IDT is an Associate Member of the Intel® Communications Alliance (www.intel.com/go/ica).
About IDT
IDT is a world leader in developing and delivering vital semiconductor solutions that enable customers to accelerate innovation. IDT solutions help customers solve complex system design challenges associated with the evolving requirements of communications, computing and consumer applications. By leveraging its system knowledge and extensive blend of technologies, IDT is able to deliver essential solutions, including timing products, network search engines, flow-control management ICs and products for standards-based serial switching. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com.
###
IDT and the IDT logo are trademarks of Integrated Device Technology, Inc. Other brands, product names and marks are trademarks, registered trademarks, or trade names of their respective owners.