SAN JOSE, Calif., February 15, 2012– Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that it has been selected as a finalist for three UBM Electronics ACE Awards presented by EE Times and EDN. IDT’s Michael S. McCorquodale, Ph.D., is nominated for the "Innovator of the Year" award, while the IDT LDS700x PureTouch® full-resolution touch controller and 3LG CystalFree™ solid-state oscillator are nominated for "Ultimate Products" awards.
Michael S. McCorquodale, Ph.D., is the general manager of the Silicon Frequency Control group at IDT and a senior member of the IEEE. McCorquodale is nominated for Innovator of the Year for his pioneering work to successfully realize the simple and highly desired concept of replacing mechanical quartz crystal oscillators with all-silicon (CMOS) oscillators.
The IDT 3LG family of ±50 ppm CrystalFree solid-state oscillators is nominated for the Ultimate Products award in the Analog IC category. The IDT 3LG crystal-oscillator (XO) replacement products save up to 75 percent power and can be used in a broad range of applications requiring a ±50 ppm timing reference, including computing, communications and consumer markets. IDT’s 3LG family of solid-state oscillators recently claimed the 2011 Product of the Year Award from Electronic Products magazine.
The IDT LDS700x PureTouch touch screen controller family is a finalist for the Ultimate Products award in the Human-machine Interface category. The LDS700x is the world’s first touch screen controller IC optimized for IDT’s proprietary single-layer multi-touch projected capacitive touch screen technology. This touch screen technology and controller offers a true single-layer solution with full multi-touch capability. The result is a lower-cost option that does not sacrifice features or performance in handheld gaming platforms, personal navigation devices and mobile handsets with screen sizes up to five inches.
To cast your vote for IDT’s products, visit the UBM ACE Awards online ballot here: http://www.surveymonkey.com/s/6H6Y9PF.
About IDT
Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.
###
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.