De-facto Industry Standard Benchmark for Testing Video Products; Orderable in Both Standard- and High-Definition Formats
January 8, 2010
SAN JOSE, Calif., January 8, 2010 – IDT® (Integrated Device Technology, Inc.; NASDAQ: IDTI), a leading provider of essential mixed signal semiconductor solutions that enrich the digital media experience, today premiers the next generation Hollywood Quality Video™ (HQV®) Benchmark DVD. The de-facto industry standard test disk has been used by journalists, reviewers and consumers worldwide as a trusted source for evaluating the picture quality, processing and performance of standard definition and high definition products including displays, DVD and Blu-ray players, A/V receivers, projectors and video processing boxes.
Building on previous Benchmarks, the HQV Benchmark 2.0 introduces advanced testing capabilities for such functions as compression artifact reduction, scaling quality and color processing. All video clips and test patterns on the Benchmark have been specifically designed to evaluate a variety of video processing tasks, which include video-de-interlacing, film-cadence detection, video-over film, motion correction, noise reduction and resolution enhancement. Moreover, the HQV Benchmark 2.0 also includes tests specific to basic device set-up, providing a one-stop testing experience. Like its predecessor, the HQV Benchmark 2.0 begins with an introduction, an overview of tests and an explanation of how the tests work. Additional details including a scorecard to assess video products are available on the www.HQV.com website.
“Consumers have more options than ever before when it comes to purchasing video and display equipment. Our HQV Benchmark 2.0 gives them an opportunity to “test-drive” before they buy,” said Ji Park, vice president and general manager of the IDT Video and Display Operation. “And with the ability to now obtain video from a wide variety of IP-based sources - which often deliver less than optimal compression and resolution - the Benchmark 2.0 allows consumers to evaluate the ability of their chosen device and its video processor to handle this new, highly demanding content.”
Pricing and Availability
The HQV Benchmark 2.0 Blu-ray DVD is orderable on www.HQV.com for a suggested retail price of $19.99 for the SD version and $24.99 for the Blu-ray version. For more information, to order a copy of the Benchmark DVD or if you are an interested in becoming a value added reseller, visit www.IDT.com/go/HQVsolutions or www.HQV.com.
With the goal of continuously improving the digital media experience, IDT integrates its fundamental semiconductor heritage with essential innovation, developing and delivering low-power, mixed signal solutions that solve customer problems. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com.
###
IDT, HQV, Hollywood Quality Video and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.