Next-Generation PCI Express Bridge Offers Lowest-Available Power Consumption
March 15, 2010
SAN JOSE, Calif., March 15, 2010 — IDT® (Integrated Device Technology, Inc.; NASDAQ: IDTI), a leading provider of essential mixed signal semiconductor solutions that enrich the digital media experience, today announced a PCI Express® (PCIe®)-to-PCI bridge tailored for the computing and consumer markets. The low power consumption and innovative features — such as its advanced buffering and queuing techniques — offered by the IDT bridge help designers improve overall system efficiency, making this device ideal for PC motherboards, PC adapter cards, multi-function printers, mobile applications and digital video recorder (DVR) cards. The new IDT bridge provides a smooth transition from legacy PCI to PCIe as applications migrate to the newer standard. Moreover, the bridge features an impressive 40-percent reduction in power consumption from alternative solutions — the lowest power consumption available in the industry.
The IDT PEB383 bridge has been designed to help IDT customers simplify board layout and manufacturability. The IDT PCIe-to-PCI bridge is tailored to match design characteristics of leading consumer processors, such as Intel and AMD, helping ensure ease of integration. In addition, the new PCIe-to-PCI bridge features the lowest latency and highest bandwidth compared to alternative solutions, resulting in the highest-quality overall system solution. The IDT PEB383 also features advanced buffering and queuing techniques, including short-term caching (STC), which provides more than a 500-percent improvement with non-posted transactions, helping improve overall system performance.
The IDT PEB383 bridge has been designed to help IDT customers simplify board layout and manufacturability. The IDT PCIe-to-PCI bridge is tailored to match design characteristics of leading consumer processors, such as Intel and AMD, helping ensure ease of integration. In addition, the new PCIe-to-PCI bridge features the lowest latency and highest bandwidth compared to alternative solutions, resulting in the highest-quality overall system solution. The IDT PEB383 also features advanced buffering and queuing techniques, including short-term caching (STC), which provides more than a 500-percent improvement with non-posted transactions, helping improve overall system performance.
“PCI Express has been fully adopted and is growing within the consumer market segment,” says Steve Peterson, Director of Intel Chipset Marketing. “For consumer designs that still require legacy PCI, the IDT PEB383 provides a smooth transition as add-in cards complete the transition from legacy PCI to PCI Express.”
The IDT PEB383 bridge features a PCIe port that provides 2.5Gbps throughput in a single lane configuration. This PCI port is a 32-bit-wide interface supporting frequencies up to 66MHz, allowing legacy devices to interface with the PCIe hierarchy. The PCI interface also offers a comprehensive feature set and 5V I/O tolerance to ensure interoperability with the earliest of PCI I/O devices, providing IDT customers with increased design flexibility.
“With the PEB383 bridge, our customers can expect complete interoperability from the PCIe interface to their existing PCI solutions,” said Mario Montana, vice president and general manger for the IDT Enterprise Computing Division. “This third-generation bridge leverages the performance characteristics of its predecessors while incorporating new techniques in power reduction to provide the most competitive consumer PCIe-to-PCI bridge in the industry.”
Pricing and Availability
The new PEB383 bridge is priced at $4.95 for 10,000 units and is available in a 14x14 millimeter 128-pin Quad Flat Pack (QFP) and a small 10x10mm 132-pin Quad Flat No-Lead (QFN) package. For additional information, visit www.IDT.com/go/PCIeBridges.
IDT provides the broadest range of high performance, low power PCI Express switching and bridging solutions targeting system interconnect, I/O expansion and protocol bridging connectivity requirements. In addition, IDT is the leading PCI Express timing solutions provider. IDT is an active member of the PCI Express special interest group (SIG), and has strategic product plans based upon the standard.
With the goal of continuously improving the digital media experience, IDT integrates its fundamental semiconductor heritage with essential innovation, developing and delivering low-power, mixed signal solutions that solve customer problems. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com.
###
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.